Error Detection (SRQ)

Other topics about Sample Programs

Overview

This sample program demonstrates how to use an SRQ to detect the occurrence of an error.

This program sets SRQs and then intentionally sends an invalid parameter to generate an error to be handled by this program. In the error handling part, this program examines the error, displays the error number and error message, and then displays the message indicating the suspension of the program. See Detecting Occurrence of an Error for this programming.

Sample Program in Excel VBA using VISA-COM

Dim Age507x As VisaComLib.FormattedIO488

Option Explicit

Implements VisaComLib.IEventHandler

 

Private Sub IEventHandler_HandleEvent(ByVal vi As VisaComLib.IEventManager, ByVal SRQevent As VisaComLib.IEvent, ByVal userHandle As Long)

  On Error Resume Next

  Dim readErr As Variant

  Dim i As Integer

  Age507x.WriteString "SYST:ERR?"

  readErr = Age507x.ReadList

  MsgBox "Error : " & readErr(0) & " , " & readErr(1), vbOKOnly, "Error occured."

  End

 

End Sub

 

Private Sub Err_Detect_Click()

  Dim gmgr As VisaComLib.ResourceManager

  Dim SRQ As VisaComLib.IEventManager

  

  Dim strdmy As String

  

  On Error GoTo CommandButton1_Error

  

  Set gmgr = New VisaComLib.ResourceManager

  

  Set Age507x = New VisaComLib.FormattedIO488

  Set Age507x.IO = gmgr.Open("GPIB0::17::INSTR")

  

  Set SRQ = Age507x.IO

  SRQ.InstallHandler EVENT_SERVICE_REQ, Me, 1, 0

  SRQ.EnableEvent EVENT_SERVICE_REQ, EVENT_HNDLR

  

  With Age507x

    .WriteString "*RST"

    .WriteString "*ESE 60"

    .WriteString "*SRE 32"

    .WriteString "*CLS"

    .WriteString "*OPC?"

    strdmy = .ReadString

  End With

  

  With Age507x

    .WriteString "CALC1:PAR:COUN 2"

    .WriteString "CALC1:PAR1:DEF S21"

    .WriteString "CALC1:PAR1:SEL"

    .WriteString "CALC1:FORM MLOG"

  

    .WriteString "CALC1:PAR2:DEF S11"

    .WriteString "CALC1:PAR2:SEL"

    .WriteString "CALC1:FORM LOG"

    .WriteString "*OPC?"

    strdmy = .ReadString

  End With

  

  SRQ.DisableEvent ALL_ENABLED_EVENTS, EVENT_ALL_MECH, 0

  

  Exit Sub

  

CommandButton1_Error:

  MsgBox "Error Occured. Error=" & vbTab & Err.Number & " , " & Err.Description

End Sub

 

Private Sub EndBtn_Click()

  End

End Sub

 

Sample Program in HT Basic (srq_err.bas)

10 DIM Buff$[9],Err_mes$[50]

20 INTEGER Err_no

30 !

40 ASSIGN @Agte507x TO 717

50 !

60 OUTPUT @Agte507x;"*ESE 60"

70 OUTPUT @Agte507x;"*SRE 32"

80 OUTPUT @Agte507x;"*CLS"

90 OUTPUT @Agte507x;"*OPC?"

100 ENTER @Agte507x;Buff$

110 !

120 ON INTR 7 GOTO Err_proc

130 ENABLE INTR 7;2

140 OUTPUT @Agte507x;":CALC1:PAR:COUN 2"

150 PRINT "Trace 1 Meas.Para: S21"

160 PRINT "Trace 1 Format : Log Mag"

170 OUTPUT @Agte507x;":CALC1:PAR1:DEF S21"

180 OUTPUT @Agte507x;":CALC1:PAR1:SEL"

190 OUTPUT @Agte507x;":CALC1:FORM MLOG"

200 PRINT "Trace 2 Meas.Para: S11"

210 PRINT "Trace 2 Format : Log Mag"

220 OUTPUT @Agte507x;":CALC1:PAR2:DEF S11"

230 OUTPUT @Agte507x;":CALC1:PAR2:SEL"

240 OUTPUT @Agte507x;":CALC1:FORM LOG"

250 OUTPUT @Agte507x;"*OPC?"

260 ENTER @Agte507x;Buff$

270 GOTO Skip_err_proc

280 Err_proc: OFF INTR 7

290 OUTPUT @Agte507x;";:SYST:ERR?"

300 ENTER @Agte507x;Err_no,Err_mes$

310 PRINT "Error occurred!!"

320 PRINT " No:";Err_no,"Description: "&Err_mes$

330 PRINT "PROGRAM INTERRUPT!!"

340 GOTO Prog_end

350 Skip_err_proc: PRINT "PROGRAM DONE."

360 Prog_end: END

Description

Line 40

Assigns a GPIB address to the I/O pass.

Lines 60 to 70

These lines enable bits 2, 3, 4 and 5 in the standard event status register and set bit 5 to 1 in the service request enable register.

Lines 80 to 100

These lines clear the status byte register, the standard event status register, and the error queue.

Lines 120 to 130

These lines set the branch target for an SRQ interrupt to enable SRQ interruptions.

Lines 140 to 260

These lines set the measurement parameters and their data formats for traces 1 and 2. An invalid parameter is given to the data format setting for trace 2, causing an error.

Lines 280 to 330

These lines define an error handler in the following way.

Lines 290 to 300: These lines retrieve the error number and error messages for the error from the error queue.

Lines 310 to 330 These lines display the message indicating the occurrence of the error, the error number, the error message, and the message showing that the program is suspended.

Line 350

Displays a closing message. Note that this message will not display unless this program is re-executed after setting a corrected parameter to the data format setting for trace 2.