Checking Firmware Revision and System Information
Other topics about Setting Control Functions
The serial number and options of the E5072A can be checked using the following procedure.
Press System > Firmware Revision.
The Firmware Revision dialog which shows the serial number and options is displayed.
To activate software option, see Activating Software Option.
The revision number and system information of the firmware installed in the E5072A can be checked using the following procedure.
Press System > Firmware Revision.
The Firmware Revision dialog is displayed.
The Storage revision of the E5072A can be checked using Windows Start Menu > My Computer > C: drive label. For example, the Storage version of the E5072A in the figure below is AT042. For more information, refer to Storage Revision History.