Other topics about Setting Control Functions
The preset function can be executed without displaying the OK and Cancel confirmation buttons.
Press System.
Click Misc Setup > Preset Setup.
Click Confirm to toggle ON (to show) and OFF (to hide) the confirmation buttons.
You can save the instrument state of the E5072A into a file in the mass storage, and then recall it with the preset function to reproduce that state.
If no user preset instrument state is stored, you cannot set the user preset function.
Press System.
Click Misc Setup > Preset Setup > State.
Use one of the following keys for the desired setting.
|
Softkey |
Function |
|
Factory |
Specifies the normal preset function. |
|
User |
Specifies the user-preset function. |
|
Cancel |
Returns to the softkey display in one upper level. |
To execute the user-preset function, you must have a preset setting file that has been saved. Follow these steps to save a preset instrument state of the E5072A.
Press Save/Recall.
Click Save State > User Pres.