Connecting External Accessories

The E5072A can be connected to external input/output devices such as printer, monitor, keyboard and mouse using any of the serial or USB ports provided in the rear or the front panel.

Other topics about Using Windows

Connecting a Printer

A printer can be connected to the E5072A using the Universal Serial Bus (USB) ports provided in the front or rear panel.

Connecting a Mouse

A mouse can be connected to the E5072A through the Universal Serial Bus (USB) ports provided in the front or rear panel.

Connecting a Monitor

A monitor can be connected to the E5072A using the External Monitor Output Terminal (Video) located in the rear panel of the E5072A.

Connecting a Keyboard

A keyboard can be connected to the E5072A through the Universal Serial Bus (USB) ports provided in the front or rear panel.