Other topics about Using Windows
On-Screen Keyboard is a utility provided by Windows that displays a virtual keyboard on the screen. It allows you to input characters without the need of a keyboard.
The E5072A does not require an external
keyboard for its operation. Users can input characters using an on-screen
keyboard in-built with the E5072A firmware.

You can use Windows native on-screen keyboard as well. To open On-Screen Keyboard:
Click Start > Accessibility On-Screen Keyboard.

Click Start > All Programs > Accessories > Accessibility > On-Screen Keyboard.