Only the Main, Sweep Timing, and Source Control commands corresponding to the Gain Compression measurement classes are documented here. The Segment Table commands are identical to the Sweep commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtab on the graphic below.
Click here to view links to Sweep commands for all Measurement Classes.