Sets and reads Gain Compression Analysis controls.
|
CALCulate:MEASure:GCMeas ANAlysis | DISCrete | [:STATe] | ENABle | XAXis |
Click a keyword to view the command details.
The calibration commands listed in this topic are supplemental to the Guided Cal commands.
CALC:MEAS:DEFine - creates a gain compression measurement.
SENS:GCSetup - Most Gain Compression settings.
CALC:MEAS:GCData - Gain Compression data commands
Gain compression data can also be saved to a *.csv file. Learn how.
See Also
|
Applicable Models: N522xB, N524xB, M9485A (Read-Write) Set and return the CW frequency for a compression analysis trace. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the GCA measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<num> |
CW frequency in Hz. Choose a frequency within the range of the gain compression channel. |
|
Examples |
CALC:MEAS2:GCM:ANAL:CWFR 1e9 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GCMeas:ANALysis:CWFRequency? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: N522xB, N524xB, M9485A (Read-Write) Sets and returns whether the CW frequency for the compression analysis trace can be set to only the discrete frequencies or provides interpolation. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the GCA measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
ON (or 1) - Discrete data points only. OFF (or 0) - Interpolated data points. |
|
Examples |
CALC:MEAS2:GCM:ANAL:ISD ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GCMeas:ANALysis:ISDisfrequency? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
Applicable Models: N522xB, N524xB, M9485A (Read-Write) Enables and disables a compression analysis trace. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the GCA measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
ON (or 1) - Enable compression analysis. OFF (or 0) - Disable compression analysis. |
|
Examples |
CALC:MEAS2:GCM:ANAL:ENAB ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GCMeas:ANALysis:ENABle? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
Applicable Models: N522xB, N524xB, M9485A (Read-Write) Sets and returns the type of data to display on the x-axis of a compression analysis trace. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the GCA measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
Data to display on X-axis. Choose from:
|
|
Examples |
CALC:MEAS2:GCM:ANAL:XAX PIN |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GCMeas:ANALysis:XAXis? |
|
Return Type |
Character |
|
PIN |
|