Learn about the Reference Osc.
See the rear-panel 10 MHz connector.
|
Applicable Models: N522xB, N523xB, N524xB, E5080A (Read-only) Applying a 10 MHz signal to the Reference Oscillator connector automatically sets the Reference Oscillator to EXTernal. This command allows you to check that it worked.
|
|
|
Examples |
SENS:ROSC:SOUR? |
|
Return Type |
Character |
|
Not applicable |
|
|
Applicable Models: M937xA, P937xA (Write-only) Set and read 10 MHz Reference Oscillator state. Note: This setting is NOT cleared with Preset. However, it does clear when the M937xA software is restarted. |
|
|
Parameters |
|
|
<state> |
Choose from the following: INTernal - Use the internal 10 MHz Reference Oscillator EXTernal - Use an external Reference Oscillator. Use SENSe:ROSCillator:SOURce:CONDition? to determine if the M937xA is locked to the external oscillator. |
|
Examples |
SENS:ROSC:SOUR INT sense:roscillator:source external |
|
Query Syntax |
Not applicable |
|
Return Type |
Not applicable |
|
INTernal |
|
|
Applicable Models: M937xA, P937xA (Read-only) Reads the 10 MHz Reference Oscillator 'locked' condition. When SENS:ROSC:SOUR is set to Internal, this command will always return "LOCKed". When SENS:ROSC:SOUR is set to External, then this function takes about 100 usec to read the state of the hardware. |
|
|
Examples |
SENS:ROSC:SOUR |
|
Return Type |
Character |
|
Not applicable |
|