When you use the M9485A and M937xA, you can control the M9161D switch through the VNA firmware. The following commands are available when the launcher includes the M9161D.
SENSe:SWITch:M9161 | COUNt? | MODule | :CHASsis | :SLOT
|
Click on a keyword to view the command details.
Applicable Models: M9485A, M937xA (Read-only) Returns the total number of M9161D switch modules that are connected to the VNA firmware. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
Examples |
SENS:SWIT:M9161:COUN? |
Return Type |
Numeric |
Default |
Not applicable |
Applicable Models: M9485A, M937xA (Read Only) Returns the chassis number where the specified M9161D module is located. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9161D. The number starts from 1 for the leftmost module of M9161D. |
Examples |
SENS:SWIT:M9161:MOD1:CHAS? sense:SWITch:m9161:module2:chassis? |
Return Type |
Numeric |
Not applicable |
Applicable Models: M9485A, M937xA (Read-Write) Sets and reads the status of M9161D control. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<mod> |
Module number of M9161D. The number starts from 1 for the leftmost module of M9161D. |
<bool> |
Module control state. Choose from: O or OFF - Skips to control the M9161D at the specified channel. 1 or ON - Enables to control the M9161D at the specified channel. |
Examples |
SENS:SWIT:M9161:MOD1:CONT ON sense2:SWITch:M9161:module2:control 0 |
Query Syntax |
SENSe<cnum>:SWITch:M9161:MODule<mod>:CONTrol[:STATe]? |
Return Type |
Boolean |
1 or ON |
Applicable Models: M9485A, M937xA (Write Only) Resets the switches in the specified module to "All Open" state immediately. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9161D. The number starts from 1 for the leftmost module of M9161D. |
Examples |
SENS:SWIT:M9161:MOD1:RES:IMM sense:SWITch:M9161:module2:reset:immediate |
Query Syntax |
Not applicable |
Return Type |
Not applicable |
Not applicable |
Applicable Models: M9485A, M937xA (Read Only) Reads the slot number where the specified M9161D is located. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9161D. The number starts from 1 for the leftmost module of M9161D. |
Examples |
SENS:SWIT:M9161:MOD1:SLOT? sense:SWITch:M9161:module2:slot? |
Return Type |
Numeric |
Not applicable |
Applicable Models: M9485A, M937xA (Read-Write) Sets and reads the path for the M9161D switch |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<mod> |
Module number of M9161D. The number starts from 1 for the leftmost module of M9161D. |
<char> |
Path. Choose from: STATe1 to STATe4 - State 1 to 4 NFRFout - NF RF Out port (NF measurement only) NFLO2 - NF LO 2 (Option 720 only) NFPort1 to NFPort24 - NF port 1 to 24 (NF measurement only) |
Examples |
SENS:SWIT:M9161:MOD1:SWIT:PATH A sense2:SWITch:M9161:module2:switch:path b |
Query Syntax |
SENSe<cnum>:SWITch:M9161:MODule<mod>:SWITch:PATH? |
Return Type |
<char> |
STATe1 |