The following settings are used to configure the analyzer for remote control using SCPI commands.
The analyzer LCL and RMT (Local and Remote) operation labels appear in the lower right corner of the status bar.
Note: The status bar is NOT visible when the analyzer is preset. See how to make the status bar visible.
LCL appears when NOT under SCPI control
RMT appears when under SCPI control. The RMT label does NOT appear when under COM control. Remote operation disables the front panel keys except for the Macro/Local key.
To return to Local (front panel) operation, press the Macro / Local key
Sending the GPIB "GTL" (go to local) command also returns the analyzer to Local operation.
Sending the GPIB "LLO" (local lockout) command disables the front panel Local button.