Operator's Check


Tip: Use Move App to Back to cause the VNA application to move behind this application on the screen.

Overview

The Operator's Check should be performed when you first receive your VNA, and any time you wish to have confidence that the VNA is working properly.

Notes

  • The Operator's Check does not verify performance to specifications. To verify VNA performance to specifications, run System Verification.

How to Run the Operator's Check

Using Hardkey/SoftTab/Softkey

  1. Press System > Service >  Operator's Check.

  1. Follow the instructions to proceed with the test.

This dialog box will look slightly different, depending on VNA model number and installed options. Some of the tests are not run if the appropriate option is not installed.

To learn about how each test is performed, click one of the tests on the right of the dialog  For example, the following information dialog is launched when Leveling is clicked:

 

Operators Check dialog box help

Note: It is normal for a momentary unleveled condition to appear during portions of the Operators Check.

Configure

Prompt for attachment of Short / Open   If you do not have enough shorts or opens for all test ports, you will be prompted to move the standard to the next test port. Connect either a short or open to port 1, then click Begin.

Shorts / Opens are attached to all ports   Connect either a short or open for each test port, then click Begin. All ports are tested without interruption. You can mix shorts and opens on the test ports.

VNA   Shows information about the VNA that is being tested.

Legend   Shows the status icons used in the Operator's Check and their meaning. Pending Pass means that a portion of the testing has been completed successfully.

Results   Shows the current status of each test. Click on the test name to learn how that test is performed. This may help in troubleshooting failed tests. If any tests Fail, refer to Chapter 3 of the VNA service guide.

Begin   Starts the Operator's Check.

View Results  Shows all results in text format.  Failed items are preceded by ===>>>.

This text file can be printed or saved with a unique file name to compare results with previous or subsequent testing.

Exit   Ends the program and closes the window.