Show 

Reverse Isolation


Reverse isolation is a measure of amplifier reverse transmission response- from output to input.

See other Tutorials

What is Reverse Isolation?

Reverse isolation is a measure of how well a signal applied to the device output is "isolated" from its input.

The measurement of reverse isolation is similar to that of forward gain, except:

The equivalent S-parameter is S12.

Why Measure Reverse Isolation?

An ideal amplifier would have infinite reverse isolation-no signal would be transmitted from the output back to the input. However, reflected signals can pass through the amplifier in the reverse direction. This unwanted reverse transmission can cause the reflected signals to interfere with the desired fundamental signal flowing in the forward direction. Therefore, reverse isolation is important to quantify.

Accuracy Considerations

Since amplifiers often exhibit high loss in the reverse direction, generally there is no need for any attenuation that may have been used to protect the port 2 receiver during forward transmission measurements. Removing the attenuation will:

The RF source power can be increased to provide more dynamic range and accuracy.

Note: With the attenuation removed and the RF source power increased, a forward sweep could damage the analyzer's port 2 receiver. Do not perform a forward sweep or use 2-port calibration unless the forward power is set low enough to avoid causing port 2 receiver compression or damage.

If the isolation of the amplifier under test is very large, the transmitted signal level may be near the noise floor or crosstalk level of the receiver. To lower the noise floor:

Note: Reducing IF bandwidth or using averaging improves measurement dynamic range and accuracy, at the expense of reduced measurement speed.

How to Measure Reverse Isolation

  1. Connect the amplifier as shown in the following graphic.

  1. Preset the analyzer.

  2. Select an S12 measurement.

  3. Select the settings for your amplifier under test.

  4. Remove the amplifier and perform a thru-response calibration or a response and isolation calibration.

  5. Scale the displayed measurement for optimum viewing and use a marker to measure the reverse isolation at a desired frequency.

  6. Print or save the data to a disk.