These commands are for setting up bandwidth tests.
| CALCulate:MEASure:BLIMit BWIDth DISPlay | MARKer | STATe REPort | DATA? | 
Click a keyword to view the command details.
See Also
| Applicable Models: All (Read-Write) Sets bandwidth threshold value (attenuation from the peak) of the bandwidth test. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <value> | Bandwidth N dB points | 
| Examples | CALC:MEAS:BLIM:BWID:THR 
		 5 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:BWIDth:THReshold? | 
| Return Type | Numeric | 
| 3 | |
| Applicable Models: All (Read-Write) Turns ON/OFF the bandwidth value display of the bandwidth test, for the active trace of selected channel. | |
| Parameters | |
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <bool> | ON or 1 - Turns limit 
		 testing ON. | 
| Examples | CALC:MEAS:BLIM:DISP:MARK:STAT 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:DISPLay:BWIDth:STATe? | 
| Return Type | Boolean | 
| OFF | |
| Applicable Models: All (Read-only) Get the bandwidth limit test results, for the active trace of selected channel. | |
| Parameters | |
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <bool> | Boolean 
 | 
| Examples | CALC:MEAS:BLIM:FAIL? | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:FAIL? | 
| Return Type | Boolean | 
| Not Applicable | |
| Applicable Models: All (Read-Write) Sets/gets the upper limit value of the bandwidth test, for the selected channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <max> | Maximum bandwidth | 
| Examples | CALC:MEAS:BLIM:MAX 
		 1E6 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:MAXimum? | 
| Return Type | Numeric | 
| 300000 | |
| Applicable Models: All (Read-Write) Sets or returns the lower limit value of the bandwidth test, for the selected channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <min> | Minimum bandwidth | 
| Examples | CALC:MEAS:BLIM:MIN 
		 1E6 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:MINimum? | 
| Return Type | Numeric | 
| 10000 | |
| Applicable Models: All (Read-only) Read the bandwidth value of the bandwidth test, for the active trace of selected channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC:MEAS:BLIM:REP:DATA? | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:REPort:DATA? | 
| Return Type | Numeric | 
| OFF | |
| Applicable Models: All (Read-Write) Turns ON/OFF the bandwidth test function, for the active trace of selected channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <bool> | ON or 1 
		 - Turns limit testing ON. | 
| Examples | CALC:MEAS:LIM:STAT 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:BLIMit:DIPLay:MARKer:STATe? | 
| Return Type | Boolean | 
| OFF | |