↵

SCPI Command Tree


See Also


ABORt

Stops all sweeps

AFR

Automatic Fixture Removal

+  CALCulate    Click to hide and show CALC SCPI command branches+  CALCulate    Click to hide and show CALC SCPI command branches

CORRection

Electrical Delay and Phase Offset

CUSTom

Custom measurements

DATA

Sends and queries data

DIQ

Differential IQ measurement

DTOPology

Defines topology for a balanced measurement

EQUation

Equation Editor

FILTer

Time domain gating

FORMat

Display format

FSIMulator

Balanced measurements and Fixturing

FSIMulator Draft

Fixture Simulator (Draft)

FSIMulator Active

Fixture Simulator (Active)

FUNCtion

Trace Statistics

GCData

Read Gain compression data

GCMeas

Gain Compression Analysis

GDELay

Group Delay Aperture setting

HOLD

Trace Hold

LIMit

Limit lines for pass / fail testing

MARKer

Marker settings

MATH

Math / Memory

MEASure

Measurement settings specific to a measurement number

    BLIMit

Bandwidth threshold settings

    COMPutation:DEViation

Trace deviation

    CONVersion

Conversion parameter setting

    CORRection

Electrical delay settings

    DATA

Sends and queries data

    DISTortion

AM Distortion

    EQUation

Equation editor trace settings

    FILTer

Gate filter settings

    FORMat

Display format settings

    FUNCtion

Trace Statistics

    GCData

Read Gain compression data

    GCMeas

Gain Compression Analysis

    GDELay

Group Delay Aperture settings

    HOLD

Trace hold settings

    LIMit

Limit line settings

    MARKer

Marker settings

    MATH

Math operations

    MIXer

X-axis display for FCA measurements

    OFFSet

Mag and Phase offset

    PARameter

Balanced measurement parameter settings

    PN

Phase Noise measurement settings

    RDATa?

Returns receiver data

    RLIMit

Ripple limit settings

    SA:MARKer

Spectrum Analyzer markers

    SMOothing

Smoothing settings

    TRANsform

Time domain transform settings

    UNCertainty

Uncertainty trace properties

    X

X-Axis settings

MIXer

X-axis display for FCA measurements

NORMalize

Receiver power cal (Obsolete)

OFFSet

Mag and Phase offset

PARameter

Create and delete measurements

RDATa?

Queries receiver data

SMOothing

Point-to-point smoothing

TDR

Enhanced Time Domain Analysis

TRANsform

Time domain transform

UNCertainty

Uncertainty Trace Properties

X:AXIS

X-Axis Domain

 

CALPod

Controls CalPod units

CONTrol

Interface control, ECal module state control, and Rear-panel connector control.

CONTrol:MULTiplexer

Control the E5092A Configurable Multiport Test Set.

CSET

Work with a Cal Set without having to select it into that channel.

DISPlay

Display settings

FORMat

Format for data transfer

HCOPy

Hardcopy printing

INITiate

Continuous or manual triggering

LLO

Local Lockout

LXI

LXI communications

MMEMory

Saves and recalls instrument states

OUTPut

Turns RF power ON and OFF

ROUTe

Controls internal switch to reference receiver. (Opt 81)

+ SENSe      Click to hide and show SENSe SCPI command branches+ SENSe      Click to hide and show SENSe SCPI command branches

AMPLifier

Control the M9379A

AVErage

Sweep Averaging

BANDwidth

IF Bandwidth

CLASs

Returns measurement class name

CORRection

Calibration and other correction settings

    | CKIT

Manage Cal Kits and ECal modules

    | COLL:CKIT

Edit Cal Kit definitions

    | COLL:GUIDed

Perform Guided Cals

    | COLL:SESSion

Perform SMC and VMC calibrations

    | CSET

Manage Cal Sets

    | EXTension

Port Extensions

    | IMD

Controls IMD and IMDx calibration

    | TDR

Enhanced Time Domain Analysis

Control

Interface Control settings

COUPle

Chopped or Alternate sweep

DIQ

Differential IQ

Distortion

Configures the modulation distortion settings.

DUTControl

Control M9341B

ECAL:CHARacterize

Ecal user characterization

FOM

Frequency Offset

FOM Segment

Construct a segment table

FREQuency

Frequency sweep settings

GCSetup

Gain Compression App 

IF

IF Access settings

IMD

Intermodulation Distortion (opt S93087A/B)

IMS

Intermodulation Spectrum (opt S93087A/B)

MIXer

FCA measurements (opts S93082A/B and S93083A/B)

MIXer Embed LO

Allows measurements of mixers with embedded LO

MIXer Segment

Configures mixer segments

MULTiplexer

Controls external test sets

NOISe

Noise Figure (opt 028 / 029)

PATH

Provides access to hardware configuration

PN

Phase Noise measurement settings

POWer

Receiver attenuation and overpower protection

PULSe

Configure internal pulse generators

ROLE

Assign sources to roles

ROSCillator

Returns the source of the reference oscillator

SA

Spectrum Analyzer settings

SEGMent

Segment sweep settings

SOURce

Receiver gain settings

SWEep

Sweep types

SWEep Pulse

Pulse measurements

SWITch

Control the M9191D switch module

TDR

Enhanced Time Domain Analysis

TEMPerature

Returns the temperature on the receiver board

VSA

Controls the connection between the VNA and the Vector Signal Analyzer (89600 VSA) Application.

X:VALues

Returns X-axis values for channel

 

SERVice

Service commands

+ SOURce    Click to hide and show SOURce SCPI command branches+ SOURce    Click to hide and show SOURce SCPI command branches

SOURce

View all Source SCPI commands

    DPD

Digital Predistortion control

    DC

DC Source control

   MODulation

Control external source to set up and calibrate I/Q modulation.

   Multi-Dimensional Sweep

Multi-dimensional sweep control on a Spectrum Analyzer channel

    PHASe

Phase control (Opt S93088A/B)

    POWer:CORR

Source power calibration

        ALC:MODE:REC

Receiver Leveling

PULSe

Enable pulse state control using external pulse source

   TDR

Enhanced Time Domain Analysis

 

STATus

Reads the VNA status registers

+ SYSTem    Click to hide and show SYSTem SCPI command branches+ SYSTem    Click to hide and show SYSTem SCPI command branches

SYSTem

View all system setting commands

    ACTive

Manage active channel/measurement

    | CAL:All

Calibrate All Channels

    | CAL:CALupdate

Contains commands used to recorrect S11 and S22 error between the VNA and the DUT reference plane.

    | CAPability

Reads various capabilities of the analyzer

    | CHANnels

Perform channel operations

    | COMMunicate

Controls and queries PNA settings

    | CONF:EDEV

Configure external devices

    | CONF:EDEV:DC

Configures external SMU, DC Meter, and DC Source properties

   | CONF:EDEV:PMAR

Configures external Power Meter as Receiver

    | FIFO

Controls data in and out of FIFO data buffer

    | PREFerences

VNA Preferences

    | SERVice

PathWave Calibration Advisor commands

    |TDR

Enhanced Time Domain Analysis

    | UNCertainty

Dynamic Uncertainty

 

TRIGger

Trigger measurements