Frequency range is the span of frequencies you specify for making a device measurement.
Auto Tune (Option S9x09xxA/B, S9x090A/B only)
Span All Meas Bands (Option S93070xB, S9x070A/B Modulation Distortion only)
See other 'Setup Measurements' topics
How to set Frequency RangeYou can also make these settings and more from the Sweep Type dialog. See the frequency ranges of all analyzer models. |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Either of the following pairs of settings determine the frequency range. The last value that you enter determines the X-Axis labels. For example, if you enter the Start and Span values, the X-Axis will show Center and Span labels. Start /Stop - Specifies the beginning and end frequency of the swept measurement range. Note: The start frequency at preset may not be the minimum value in full range. Note: The maximum frequency of E5080B 2P0, 2P2, 4P0. 4P2 is 54 GHz. However, the specification is applied up to 53 GHz.( The maximum frequency is 53 GHz for the units shipped with the A.13.70 and below. Re-calibration is required for upgrade.) Center /Span - Specifies the value at the center and frequency range. Either of the following settings determine the number of evenly-spaced data points across the frequency range. Points - Specifies the number of evenly-spaced data points across the frequency range. Learn more about Data Points. Step - Available ONLY in Linear sweep type. Specifies the frequency step size between evenly-spaced data points. Changes to this setting will cause the Points setting to adjust to the closest integer. Any 'remainder' will adjust either the Stop value or Span value depending on which is displayed on the X-Axis label. |
|
Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.
Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.
How to Zoom in a measurement window |
Notes
Zoom is NOT available for the following:
|
Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.
How to set CW Frequency |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
CW Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the VNA. |
The resolution for setting frequency is 1 Hz.
The Auto Tune softkey is a feature of the Spectrum Analyzer measurement class (Option S9x09xxA/B, S9x090A/B). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.
The Span All Meas Bands softkey is a feature of the Modulation Distortion measurement class (Option S93070xB, S9x070A/B only). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.