Print a Displayed Measurement


The analyzer allows you to print a displayed measurement to a printer or to a file. The printer can be either networked or local.

Other Outputting Data topics

Connecting a Printer

You can connect a printer to one of the VNA USB ports or to the LAN connector.

To Add a Printer

Note: If you try to print from the VNA application and the Add Printer Wizard appears, click Cancel and add the printer using the following procedure.

  1. From the VNA application, press System > Main > Minimize Application.

  2. On the Windows taskbar, click Devices and Printers.

  3. Double-click Add Printer.

  4. Follow the instructions in the Add Printer Wizard.

For more information, refer to Microsoft Windows Help or your printer documentation.

Printing

The measurement information on the screen can be printed to any local or networked printer that is connected to the VNA. The graphic below shows an example of how a screen-capture image appears when printed. The Page Setup settings allows you to customize the printed form of the measurement information.

 

How to Print a Hardcopy

Using Hardkey/SoftTab/Softkey

  1. Press System > Print.

  2. Click Print....

No programming commands are available for this feature.

Note: For information on the choices in the Print dialog box, see Windows Help.

Page Setup

The Page Setup dialog allows flexibility in the appearance that measurement data is printed. After setting up the page, click File, then Print... to obtain a hard-copy.

How to select Page Setup

Using Hardkey/SoftTab/Softkey

  1. Press System > Print > Page Setup....

OR

    1. Press System > System Setup > Preferences.....
    2. Click the Page Setup... button on Preferences dialog box.

Programming Commands

Page Setup dialog box help

Paper, Orientation, and Margins

These settings do NOT survive a VNA shutdown.

See Windows Help for information on these settings.

Windows

The following VNA-specific settings DO survive a VNA shutdown:

Minimum vertical size  Adjust to change the amount of a page that the measurement window fills. The adjustment range is from 40 to 100%.

One window per page  Check to print one window per page. Clear to print all selected windows without a forced page break.

Only active window  Check to print only the active window. Clear to print all windows.

Instrument logo  Check to print the Keysight logo to the header.

Data and Time  Check to add the current date and time to the header.

Global Pass/Fail  Check to add the Global Pass/Fail status to the header.

Page Numbers  Check to add page numbers (1 of n) to the header.

Channel Settings Table

Print  Check to print the channel settings table.

Segment data can no longer be printed.

Trace Attributes Table

Print  Check to print the Trace Attributes Table. The Trace Attributes are measurement type, correction factors ON or OFF, smoothing, options, and marker details. The Trace Attributes are listed by Trace ID#  for each window.

Each Trace ID# can have multiple entries depending on the number of markers associated with the trace. The marker details are marker number, position and response. If there are multiple markers on a trace, the trace attributes are only shown for the first marker. However, the trace attributes for the first marker apply to all other markers on that trace.

The options column can have one or more options. D for Delay, M for Marker, G for Gating. Multiple options selected would appear as follows: DMG.

Print marker data  Check to print all marker data. The amount of data depends on how many markers are created.

Print to a File

The analyzer can save a screen-capture image in any of the following formats:

The analyzer automatically saves the file to the current path. If not previously defined, the analyzer automatically selects the default path D:\.

A .bmp file, like a .prn file, can be imported into software applications such as Microsoft Excel, Word, or Paint to display a screen-capture image.

See Save and Recall files for more information.

How to Print to a File

Using Hardkey/SoftTab/Softkey

  1. Press System > Print > Print to File....

Programming Commands