FETCh:CFDTune?

Last Updated: August 29, 2007

These commands return the results for the Fast Device Tune (CFDT) measurement

For more information on the conventions used in the programming examples click here.

FETCh:CFDTune[:ALL]?

Queries the Fast Device Tune Integrity Indicator, Number of Frequency Steps, Number of Power Steps, Total Number of Steps, and up to 400 MS Transmitter Power Results.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.04 and above

Example:

' Query for the integrity, number of frequency steps, total number of steps, number of results
' and the actual results.

TestSet.WriteString("FETCh:CFDTune?")

FETCh:CFDTune:ICOunt?

Queries the progress indicator. The progress indicator shows how many steps have been completed in a single Fast Device Tune measurement; it is updated approximately every 50 steps until all measurements are complete.

Query Range: <nr1>

Test Set Requirements: E6601A WCTS Program Version A.04 and above

Example:

' Query the progress indicator.

TestSet.WriteString("FETCh:CFDTune:ICOunt?")

FETCh:CFDTune:INTegrity?

Queries the Fast Device Tune integrity indicator.

Query Range: See Measurement Integrity Indicator.

Test Set Requirements: E6601A WCTS Program Version A.04 and above

Example:

' Query the integrity indicator for the Fast Device Tune measurement.

TestSet.WriteString("FETCh:CFDTune:INTegrity?")

FETCh:CFDTune:RESult:COUNt[:STEP]?

Queries the total number of steps.

Setting Range: (frequency step index) 1 to 400, (power step index)1 to 400

Query Range: <nr1>

Test Set Requirements: E6601A WCTS Program Version A.04 and above

Example:

' Query the total number of steps.

TestSet.WriteString("FETCh:CFDTune:RESult:COUNt?")

FETCh:CFDTune:TRACe:POWer?

Queries the Fast Device Tune Integrity Indicator and the Power Step Results for the specified step indexes. To specify the Power Step Results you want the test set to return, you must list both the Frequency Step and the Power Step for each result. You must specify at least one power frequency and power step for this command.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.04 and above

Example:

' Query the Fast Device Tune measurement integrity and the first and second Power Step Results for Frequency Steps 1 through 3.

TestSet.WriteString("FETCh:CFDTune:TRACe:POWer? 1,1,1,2,2,1,2,2,3,1,3,2")