RF Analyzer

Last Updated: August 29, 2007

The RF Analyzer tab on the RF Control window provides access to the RF Analyzer (receiver) parameters.

Control Mode

This parameter sets the RF analyzer frequency control mode, either Auto or Manual. When set to Manual, you can specify the RF analyzer frequency.

SCPI command: RFANalyzer:CONTrol:FREQuency:AUTO:CCALibration[?]

Band Class

This parameter sets the RF generator's band class. See Supported Band Classes for details on which band classes are supported by the test set.

SCPI command: TRANsceiver:BAND:CCALibration[?]

Channel

This parameter sets the physical channel number for the specified band class.

SCPI command: TRANsceiver:CHANnel[:SELected]:CCALibration[?]  

Frequency

This parameter sets the manual frequency of the RF analyzer.  

SCPI command: RFANalyzer:MANual:FREQuency:CCALibration[?]

System Type

This parameter sets type of cell the system is emulating; cdma2000 or 1xEV-DO.

SCPI command: RFANalyzer:SYSTem:TYPE:CCALibration[?]

Expected Power

This parameter sets the power level in dBm that the test set's RF analyzer is expecting the wireless device burst to transmit at.

SCPI command: RFANalyzer:MANual:POWer[:AMPLitude]:CCALibration[?]