SCPI commands

Last Updated: August 29, 2007

This book provides details of the SCPI Commands in the E6833A cdma2000/1xEV-DO Cal Application. For details of these commands refer to the subsystems in this section. Alternatively, for a complete list of the SCPI commands in this application, see Listing of Commands (cdma2000/1xEV-DO CA).

Measurement Control

IEEE 488.2 Common Commands

RF Control