Listing of Commands

Last Updated: August 29, 2007

This topic lists all of the available SCPI commands in the E6833A cdma2000/1xEV-DO Cal Application.

It is recommended that you print this topic because it provides a useful syntax reference for all of the available cdma2000/1xEV-DO Cal Application commands. To print:

The SCPI commands in this topic are categorized by subsystem:

ABORt Subsystem

CALCulate Subsystem

DISPlay Subsystem

FETCh Subsystem

INITiate Subsystem

RFANalyzer Subsystem

RFGenerator Subsystem

SETup Subsystem

TRANsceiver Subsystem

 

Related Topics