Last Updated: August 29, 2007
This topic describes the Channel Power measurement. Channel Power is a measurement in the RF Channel measurement suite.
The Channel Power measurement measures the filtered average and peak envelope power over the measurement interval you specify.
For more information refer to How are the Measurements in the RF Channel Measurement Suite Made?.
Channel Power is a measurement in the RF Channel measurement suite. See RF Channel Measurement Suite Measurement Parameters for details of the parameters that apply to all measurements in the suite.
This result provides the integrity indicator for the RF Channel measurement suite. Normal indicates that the measurement suite completed successfully without error and the result is accurate. For details of other integrity indicators, see Measurement Integrity Indicator.
SCPI command: FETCh:RFCHannel:INTegrity?
This result provides the average channel power in dBm.
SCPI commands: FETCh:RFCHannel:CPOWer?, FETCh:RFCHannel:CPOWer:ALL?, FETCh:RFCHannel:CPOWer:AVERage?, FETCh:RFCHannel:CPOWer:AVERage:ALL?
This result provides the average channel power in dBm.
SCPI commands: FETCh:RFCHannel:CPOWer?, FETCh:RFCHannel:CPOWer:ALL?, FETCh:RFCHannel:CPOWer:PEAK?, FETCh:RFCHannel:CPOWer:PEAK:ALL?
Channel Power is a measurement in the RF Channel measurement suite. See RF Channel Input Signal Requirements for details of the input signal requirements that apply to all measurements in the suite.