FETCh:ORFSpectrum? Common Results

Last Updated: August 29, 2007

These commands return results that are applicable to the entire Output RF Spectrum (ORFS) measurement suite.

For more information on the conventions used in the programming examples click here.

FETCh:ORFSpectrum[:PARTial]?

Queries the ORFS measurement suite integrity, ORFS measurement suite overall pass/fail result, TX carrier power, ORFS Switching number of fetch points, up to eight comma-separated ORFS Switching (maximum) results, 30 kHz reference power, ORFS Modulation number of fetch points, and up to 22 ORFS Modulation (average) results.

The ORFS Switching number of fetch points, and the ORFS Modulation number of fetch points return a 1 when there are no points, to indicate that one value of 9.91 E+37 (NAN) will be returned.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the partial results for the entire ORFS measurement suite.

TestSet.WriteString("FETCh:ORFSpectrum?")

FETCh:ORFSpectrum:FAIL?

Queries the ORFS measurement suite integrity indicator and overall pass/fail result.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the ORFS measurement suite overall pass/fail result.

TestSet.WriteString("FETCh:ORFSpectrum:FAIL?")

FETCh:ORFSpectrum:ICOunt?

Queries the intermediate total number of bursts measured. Refer to the following example return values:

Query Range: 0 to 999

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Queries the intermediate total number of averages completed in the ORFS measurement suite.

TestSet.WriteString("FETCh:ORFSpectrum:ICOunt?")

FETCh:ORFSpectrum:INTegrity?

Queries the integrity indicator for the last Power and Modulation Quality measurement suite completed. Zero indicates normal.

For non-zero integrity indicators, refer to Measurement Integrity Indicator.

Query Range: See Measurement Integrity Indicator.

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the integrity indicator for the last Output RF Spectrum measurement suite completed.

TestSet.WriteString("FETCh:ORFSpectrum:INTegrity?")

FETCh:ORFSpectrum:TXPower?

Returns the integrity indicator and the TX carrier power measurement result from the last ORFS measurement made.

Query Range:  

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the TX carrier power from the last ORFS measurement.

TestSet.WriteString("FETCh:ORFSpectrum:TXPower?")