QPSK EVM (EVMQ) Measurement Description

Last Updated: August 29, 2007

This topic describes the QPSK EVM measurement. QPSK EVM is a measurement in the RF Channel measurement suite.

How is a QPSK EVM Measurement Made?

This measurement allows you to measure a QPSK (quadrature phase-shift keying) modulated signal's error vector magnitude (EVM). This can be used to verify the performance of the wireless device's transmitter.

3GPP TS 34.121 section 5.13 states "The Error Vector Magnitude is a measure of the difference between the reference waveform and the measured waveform. This difference is called the error vector. Both waveforms pass through a matched Root Raised Cosine filter with bandwidth 3.84 MHz and roll-off alpha =0.22. Both waveforms are then further modified by selecting the frequency, absolute phase, absolute amplitude and chip clock timing so as to minimise the error vector. The EVM result is defined as the square root of the ratio of the mean error vector power to the mean reference power expressed as a %."

The EVM measurement in the test set compares the received signal's IQ modulation characteristics to an ideal signal, as defined in 3GPP TS 34.121 section 5.13 and annex B. As can be seen in the figure below, the error vector is the difference between the measured signal and reference signal.

Figure 1: Error Vector

The two main differences between this measurement and the WCDMA Error Vector Magnitude (EVM) Measurement, the cdma2000/1xEV-DO Waveform Quality Measurement and the TD-SCDMA Error Vector Magnitude (EVM) Measurement are:

This measurement requires you to use the 5 MHz filter setting.

 For more information refer to How are the Measurements in the RF Channel Measurement Suite Made?.

QPSK EVM Measurement Parameters

QPSK EVM is a measurement in the RF Channel measurement suite. See RF Channel Measurement Suite Setup Parameters for details of the parameters that apply to all measurements in the suite.

QPSK EVM Measurement Results

Integrity Indicator

This result provides the integrity indicator for the RF Channel measurement suite. Normal indicates that the measurement suite completed successfully without error and the result is accurate. For details of other integrity indicators, see Measurement Integrity Indicator.

SCPI command: FETCh:RFCHannel:INTegrity?

EVM (rms)

This result provides the Error Vector Magnitude in % rms. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command:  FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

EVM (peak)

This result provides the peak Error Vector Magnitude in %. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command: FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

Phase Error

This result provides the phase error in degrees. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command: FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

Magnitude Error

This result provides the magnitude error in %. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command: FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

Frequency Error

This result provides the frequency error in Hz. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command: FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

Origin Offset

This result provides the origin offset (distance away from the origin) in dB. If the Multi-Measurement Count is enabled, the average, minimum, maximum and standard deviation results are returned, otherwise the single measurement result is returned.

SCPI command: FETCh:RFCHannel:EVMQpsk[:PARTial]?, FETCh:RFCHannel:EVMQpsk:ALL?

QPSK EVM Tab

The measurement results are available on the RF Channel Suite's QPSK EVM tab as shown below. (Note, to display the  QPSK EVM tab, the measurement must be enabled in the RF Channel Suite Setup window's Results Configuration tab.)

These results are also displayed on the RF Channel Suite's Summary tab if the measurement is enabled.

QPSK EVM Input Signal Requirements

QPSK EVM is a measurement in the RF Channel measurement suite. See RF Channel Input Signal Requirements for details of the input signal requirements that apply to all measurements in the suite.   

 

Related Topics