Last Updated: August 29, 2007
The RF Generator tab on the RF Control window provides access to the RF Generator (source) parameters.
This parameter sets the RF generator frequency control mode, either Auto or Manual. When set to Manual, you can specify the RF generator frequency.
SCPI command: RFGenerator:CONTrol:FREQuency:AUTO:GCALibration[?]
This parameter sets the RF generator frequency.
SCPI command: RFGenerator:FREQuency:GCALibration[?]
This parameter sets the GSM/GPRS band. The test set's RF source and RF analyzer are automatically set to the appropriate frequencies for the band you specify.
SCPI command: TRANsceiver:BAND:GCALibration[?]
This parameter sets the ARFCN for the currently selected GSM/GPRS band.
SCPI command: TRANsceiver:CHANnel(:DCS|:EGSM|:GSM450|:GSM480|:GSM750|:GSM850|:PCS|:PGSM|:RGSM)[?]
This parameter performs two functions: (1) sets the RF generator power level and (2) sets the RF generator power state to on or off.
SCPI command: RFGenerator:POWer[:SAMPlitude]:GCALibration[?]
This parameter sets the RF generator modulation mode. The following selections are available:
Continuous wave (CW)
Amplitude modulation (AM)
Frequency modulation (FM)
Double sideband suppressed carrier (DSB-SC)
Arbitrary waveform generator (ARB)
SCPI command: RFGenerator:MODulation:GCALibration[?]
This parameter sets the RF generator modulation frequency. This setting only applies when the modulation mode is set to AM, FM, or DSB-SC.
SCPI command: RFGenerator:MODulation:FREQuency:GCALibration[?]
This parameter sets the RF generator AM depth. This setting only applies when the modulation mode is set to AM.
SCPI command: RFGenerator:AM:DEPTh:GCALibration[?]
This parameter sets the RF generator FM deviation. This setting only applies when the modulation mode is set to FM.
SCPI command: RFGenerator:MODulation:FM:DEViation:GCALibration[?]
This parameter sets the arbitrary waveform (ARB) file from the ARB random access memory (RAM) disk directory.
When a file is selected it is loaded into the ARB memory so that it can be run.
The following waveforms are available:
GSM_Bch7Dummys
This waveform comprises of: a BCH on slot zero; slots 1-7 are dummy
bursts; and the file is 208 frames in length.
GSM_Bch7Normals
This waveform comprises of: a BCH on slot zero; slots 1-7 are normal
bursts; and the file is 208 frames in length.
EGPRS_TSC5
This waveform comprises of: an EGPRS TSC5 normal burst on slot zero;
slots 1-7 are off; and the file is 1 frame in length.
In all these waveforms the data sections contain random data.
SCPI command: RFGenerator:AWAVeform:SELection
This parameter sets the ARB run mode. Setting this command to:
Run starts running the ARB file from the beginning.
Stop provides no output and turns the TSP IF off.
SCPI command: RFGenerator:AWAVeform:RUN[?]
This parameter sets the external ARB output trigger. The external trigger drives the rear panel BBP TRIG OUT BNC connector.
SCPI command: RFGenerator:AWAVeform:TRIGger:EXTernal[:OUTput][?]
This parameter sets the RF output port destination: RF In/Out or RF Out Only.
SCPI command: RFGenerator:OUTPut[:DESTination]