SETup:PMODulation:TXPower

Last Updated: August 29, 2007

This command sets a parameter for the Transmit Power measurement in the Power and Modulation Quality (PMOD) measurement suite.

For more information on the conventions used in the programming examples click here.

SETup:PMODulation:TXPower:METHod[?]

For an 8PSK burst, this command specifies whether the measured power is based on the estimated carrier power or the average power during the useful part of the burst.

For a GMSK burst, this parameter has no effect.

Setting Range: CARRier | BURSt

Query Range: CARR | BURS

*RST Setting: CARRier

Test Set Requirements: E6601A WCTS Program Version A.03 and above

Example:

' Set the measured power to be based on the estimated carrier power

TestSet.WriteString("SETup:PMODulation:TXPower:METHod CARRier")