Last Updated: August 29, 2007
These commands return results for the Frequency Error measurement in the RF Channel (RFCH) measurement suite.
For more information on the conventions used in the programming examples click here.
Queries the integrity indicator and the average frequency error.
If the multi-measurement state is on, the results represent the average of a number of frequency error measurements. Multi-measurement state, by default, is off. To set up multi-measurements, see SETup:RFCHannel:COUNt:NUMBer[?].
Query Range:
RF Channel measurement suite integrity: See Measurement Integrity Indicator.
Frequency error (average): <nr3> in Hz and 9.91 E+37 (NAN)
Test Set Requirements: E6601A WCTS Program Version A.01 and above
Example:
' Query the integrity indicator and the average frequency error.
TestSet.WriteString("FETCh:RFCHannel:FERRor?")
Queries the integrity indicator, minimum, maximum, average, and standard deviation of frequency error multi-measurement results. To set the number of measurements used to gather statistics, use the command SETup:RFCHannel:COUNt:NUMBer[?].
Query Range:
RF Channel measurement suite integrity: See Measurement Integrity Indicator.
Frequency error (minimum): <nr3> in Hz and 9.91 E+37 (NAN)
Frequency error (maximum): <nr3> in Hz and 9.91 E+37 (NAN)
Frequency error (average): <nr3> in Hz and 9.91 E+37 (NAN)
Frequency error (standard deviation): <nr3> in Hz and 9.91 E+37 (NAN)
Test Set Requirements: E6601A WCTS Program Version A.01 and above
Example:
' Query the integrity indicator, minimum,
maximum, average, and standard deviation
' of frequency error multi-measurement results.
TestSet.WriteString("FETCh:RFCHannel:FERRor:ALL?")