SCPI Commands

Last Updated: August 29, 2007

This book provides details of the test set (platform) SCPI commands. These SCPI commands control test set configuration that is applicable to all applications that run on the test set. Application-specific SCPI commands are described in different sections of this help file such as SCPI Commands (General Purpose).

For a complete list of the test set (platform) SCPI commands, see Listing of Commands (Test Set).

Test Set Configuration

IEEE 488.2 Common Commands