Listing of Commands

Last Updated: August 29, 2007

This topic lists all of the available test set (platform) SCPI commands in the E6601A Wireless Communications Test Set. These SCPI commands control test set configuration that is applicable to all applications that run on the test set. Application-specific SCPI commands are described in different sections of this help file such as SCPI Commands (General Purpose).

It is recommended that you print this topic because it provides a useful syntax reference for all of the available test set (platform) commands. To print:

The SCPI commands in this topic are categorized by subsystem:

DISPlay Subsystem

MMEMory Subsystem

SYSTem Subsystem

 

Related Topics