SYSTem:APPLication

Last Updated: August 29, 2007

This command sets and queries test set application parameters.

For more information on the conventions used in the programming examples click here.

SYSTem:APPLication[:NAME][?]

Switches between licensed applications.

Queries the test set for the name of the currently active application.

Setting Range: CCAL | GCAL | TCAL | WCAL | GENeral | TOOLs

Query Range: CCAL | GCAL | TCAL | WCAL | GEN | TOOL

Test Set Requirements: E6601A WCTS Program Version A.01 and above

Examples:

' Switch to the GSM/GPRS/EGPRS Cal Application.

TestSet.WriteString("SYSTem:APPLication GCAL")

 

' Return the name of the currently active application.

TestSet.WriteString("SYSTem:APPLication?")