Last Updated: August 29, 2007
This command aborts all measurements.
For more information on the conventions used in the programming examples click here.
Sets all measurements to abort, if the trigger arm is set to continuous the measurements will begin a new measurement cycle.
Any measurement results are cleared and the Integrity Indicator is set to 1 (No Result Available). See Measurement Integrity Indicator.
Test Set Requirements: E6601A WCTS Program Version A.01 and above
Example:
' Abort all measurements.
TestSet.WriteString("SYSTem:MEASurement:RESet")