SYSTem:SYNChronized?

Last Updated: August 29, 2007

This command performs operations on sequential and overlapped commands.

For more information on the conventions used in the programming examples click here.

SYSTem:SYNChronized?

Queries the test set to ensure that all prior sequential commands have completed and all prior overlapped commands have started indicating that the input buffer is synchronized.

Query Range: 0 | 1

Test Set Requirements: E6601A WCTS Program Version A.01 and above

Example:

' Query the test set to ensure that the input buffer is synchronized.

TestSet.WriteString("SYSTem:SYNChronized?")