SYSTem:VERSion?

Last Updated: August 29, 2007

For more information on the conventions used in the programming examples click here.

SYSTem:VERSion?

Queries the version number of the currently running E6601A WCTS program.

Query Range: <letter>.XX.XX (where X is an integer between 0 and 9)

Test Set Requirements: E6601A WCTS Program Version A.01 and above

Example:

' Query the version number of the currently running E6601A WCTS program.

TestSet.WriteString("SYSTem:VERSion?")