Using the Test Set with a Mouse and Keyboard

Last Updated: August 29, 2007

There are many ways to perform the same actions when using the test set manually. This topic provides step-by-step procedures that are optimized for use when a USB mouse and keyboard are connected to the test set.  

With a USB mouse and keyboard connected to the test set, you can interact with the test set in the same way you would operate a desktop computer. It is recommended that you ensure a proper working environment (see Working in Comfort). Many of the functions that you can perform using the test set's front panel keys are duplicated on the graphical user interface to reduce the need for you to interact with the test set's front panel directly. For example, the application's Menu bar enables you to change screens, switch between open windows, select measurements, perform preset operations, or access the Help (see the following graphic).

 

Refer to one of the following procedures:   

To Select a Different Screen

On the Screens menu, click the screen you want.

To Select Measurements

  1. On the Measurements menu, click Measurement Selection.

  2. In the Measurement Selection window, select the measurements you want to activate, or clear the measurements you want to deactivate.

To Set Up the Selected Measurement

  1. Ensure that the results window for the measurement you want to set up is the active window.

  2. Click the Setup softkey for the measurement (for example, Spectrum Monitor Setup). The measurement's setup window opens.

  3. Set up the measurement parameters as required.

To Move Between the Application's Windows

Perform one of the following actions:

To Increase the Size of a Window

Perform one of the following actions:

Note that for some types of windows, resizing the window using a mouse is a temporary action. The window is restored to its original size when another front panel action is performed.

To Turn On or Off the State of a Parameter

For numeric parameters that also support the On/Off state:

To Switch a Parameter to Auto or Manual

For numeric parameters that also support the Auto/Manual state:

To Perform a Full or Partial Preset

On the Utility menu, click the type of preset you want, Full Preset or Partial Preset.

To Open the Help

Perform one of the following actions:

To View SCPI Syntax for a Parameter

Position the pointer at the parameter you want, right-click on the parameter box to open the pop-up (shortcut) menu, and then click SCPI Command. The SCPI syntax for the parameter is displayed on the lower status bar.

To View Application and Test Set Information

On the Help menu, click About. This displays the About E6601A Wireless Communications Test Set window containing software version and test set serial number information.

To Select a Softkey

Click on the softkey you want.

To Exit the Test Set Application

On the File menu, click Exit.

 

Related Topics