Power Supply Diagnostics

Last Updated: August 29, 2007

The Midplane board has a number of diagnostic LEDs that are visible when the outer cover is removed.

The table below lists the Power Supply Diagnostic LEDs. When the Power Supply is operating correctly the diagnostic LEDs will match the conditions indicated in the table.

Voltage

LEDs (Stand-By)

LEDs (Test Set On)

+15.0VA

Red

Off

+9.0VA

Red

Off

+3.3VA

Red

Off

+5.2VA

Red

Off

+15VSB

Green

Green

+32VA

Red

Off

-12VD

Red

Off

-15VA

Red

Off

-5.2VA

Red

Off

-7.0VA

Red

Off

+5.1VSB

Green

Green

+12VD

Red

Off

+3.35VD

Red

Off

+5.1VD

Red

Off

POWER OK

Red

Off

POWER ON

Off

Green

VA = Voltage Analog

VD = Voltage Digital

VSB = Voltage Stand By

The +15V Stand-By powers the oven controlled oscillator for 10 MHz Timebase Reference, ambient temperature sensor, power temperature shut-down circuit and the fan speed control voltage circuit. This supply is active when the test set is connected to an AC source.

The +5.1 V Stand-By powers the Advanced Configuration and Power Interface of the PC Processor, the standby power indicator on the front panel and the Power Supply Diagnostic LEDs on the Midplane Board. This supply is active when the test set is connected to an AC source.

 

Midplane Board

 

Related Topics