Adjacent Channel Leakage Ratio (ACLR) Measurement Description

Last Updated: August 29, 2007

This topic describes the Adjacent Channel Leakage Ratio measurement. Adjacent Channel Leakage Ratio is a measurement in the Dedicated Physical Channel measurement suite.

How is an Adjacent Channel Leakage Ratio Measurement Made?

The Adjacent Channel Leakage Ratio (ACLR) measurement measures the ratio of the RRC Filtered Mean Power centered on the adjacent channel frequency to the RRC filtered mean power centered on the assigned channel frequency. The adjacent channels are located at ±1.6 MHz and ±3.2 MHz offsets.

The ACLR measurement is defined in the 3GPP standards in TS 34.122 section 5.5.2.2.

Note: This measurement automatically runs the RRC Filtered Mean Power measurement, so there is no need to run the RRC Filtered Mean Power measurement while you are running the ACLR measurement.

Adjacent Channel Leakage Ratio Measurement Parameters

Adjacent Channel Leakage Ratio is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Parameters for details of the parameters that apply to measurements in the suite.

Adjacent Channel Leakage Ratio Measurement Limits

Adjacent Channel Leakage Ratio is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Limits for details of the limits parameters that apply to measurements in the suite.

Adjacent Channel Leakage Ratio Measurement Results

Integrity Indicator

This result provides the integrity indicator for the Dedicated Physical Channel measurement suite. Normal indicates that the measurement suite completed successfully without error and the result is accurate. For details of other integrity indicators, see Measurement Integrity Indicator.

SCPI command: FETCh:TDPChannel:INTegrity?

ACLR Overall Pass/Fail

This result provides the overall pass/fail for the measurement.

SCPI commands: FETCh:TDPChannel:ACLRatio[:BURSt[1]][:PARTial]?, FETCh:TDPChannel:ACLRatio[:BURSt[1]]:ALL?  

In-Channel Power

This result provides the in-channel power in dBm/1.28 MHz.

SCPI commands: FETCh:TDPChannel:ACLRatio[:BURSt[1]]:ALL?

Pass/Fail, Level, and Margin for each Offset

These results provide the pass/fail, average level, and mask margin results for the -3.2 MHz, -1.6 MHz, 1.6 MHz, and 3.2 MHz offsets.   

SCPI commands: FETCh:TDPChannel:ACLRatio[:BURSt[1]]:LOWer:ADJacent?, FETCh:TDPChannel:ACLRatio[:BURSt[1]]:LOWer:ALTernate?, FETCh:TDPChannel:ACLRatio[:BURSt[1]]:UPPer:ADJacent?, FETCh:TDPChannel:ACLRatio[:BURSt[1]]:UPPer:ALTernate?  

Adjacent Channel Leakage Ratio Input Signal Requirements

Adjacent Channel Leakage Ratio is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Input Signal Requirements for details of the input signal requirements that apply to all measurements in the suite.   

 

Related Topics