FETCh:RFCHannel?  Common Results

Last Updated: August 29, 2007

This command returns a result that is applicable to the entire RF Channel (RFCH) measurement suite.

For more information on the conventions used in the programming examples click here.

FETCh:RFCHannel:ICOunt?

Queries the intermediate count of RF Channel multi-measurements completed.

Query Range: 0 to 999

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Queries the intermediate total number of measurements completed in the RF Channel measurement suite.

TestSet.WriteString("FETCh:RFCHannel:ICOunt?")

FETCh:RFCHannel:INTegrity?

Queries the integrity indicator for the last RF Channel measurement suite completed. Zero indicates normal.

For non-zero integrity indicators, refer to Measurement Integrity Indicator.

Query Range: See Measurement Integrity Indicator.

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Query the integrity indicator for the last RF Channel measurement suite completed.

TestSet.WriteString("FETCh:RFCHannel:INTegrity?")