SETup:ALL

Last Updated: August 29, 2007

These commands set the trigger state for all measurements in this application.

For more information on the conventions used in the programming examples click here.

SETup:ALL:CONTinuous:OFF

Sets all measurements in this application to Single trigger mode. See Triggering of Measurements.

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Set all measurements in this application to Single trigger mode.

TestSet.WriteString("SETup:ALL:CONTinuous:OFF")

SETup:ALL:CONTinuous:ON

Sets all measurements in this application to Continuous trigger mode. See Triggering of Measurements.

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Set all measurements in this application to Continuous trigger mode.

TestSet.WriteString("SETup:ALL:CONTinuous:ON")