SETup:GPMeas

Last Updated: August 29, 2007

These commands set parameters that are only applicable to the General Purpose Application's measurements, that is the Dynamic Power RF Channel, and Spectrum Monitor measurements.

SETup:GPMeas:CFACtor[:SELected][?]
SETup:GPMeas:CFACtor:TCALibration[?]

Sets/queries the crest factor for the Dynamic Power, RF Channel, and Spectrum Monitor measurements. The crest factor allows the test set to range correctly and therefore helps prevent over-ranging. The higher the crest factor the less likely that an over-range will occur, however the dynamic range is decreased.

This is the only General Purpose Application parameter that can be set differently for each application, for example in the TD-SCDMA Cal Application you can use SETup:GPMeas:CFACtor:TCALibration[?]. The default crest factor is different in some applications. For more information on setting the crest factor for other applications or the defaults refer to the SETup:GPMeas:CFACtor[:SELected][?] commands detailed for the other applications.

The optional [:SELected] keyword specifies that the setting or query applies to the currently selected application. The TCALibration keyword specifies that the setting or query applies to the TD-SCDMA Cal Application.

Setting Range: 0 to 20 dB

Query Range: 0 to 20 dB

*RST Setting: 7 dB

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Set the crest factor for the General Purpose measurements in the selected application to 0.

TestSet.WriteString("SETup:GPMeas:CFACtor 0")