SETup Subsystem

Last Updated: August 29, 2007

Description

The SETup subsystem is used to configure the test set for each measurement, Typical settings include:

Trigger arming for each measurement is controlled in the SETup subsystem. The choices are single or continuous. In most cases, it is a best practice (during remote operation) to use "single" measurement mode. This simplifies the tasks of starting concurrent measurements, using the INIT subsystem commands to determine which measurements are ready to be fetched, then using the FETCh subsystem to obtain results. The command SETup:CONTinuous:OFF sets all measurements to "single" trigger mode.

For details of the SETup commands refer to the SETup subsystems in this section.