Last Updated: August 29, 2007
These commands allow you to set and query the Spectrum Emission Mask (SEM) settings associated with the Dedicated Physical Channel (DPCH) measurement suite.
For more information on the conventions used in the programming examples click here.
Sets/queries the frequency spacing between measurements for the 30 kHz and 1 MHz filters in the Spectrum Emission Mask measurement.
Setting Range: Depends upon the filter:
30 kHz filter: KHZ1 | KHZ5 | KHZ10
1 MHz filter: KHZ50 | KHZ100 | KHZ200
Query Range: Depends upon the filter:
30 kHz filter: KHZ1 | KHZ5 | KHZ10
1 MHz filter: KHZ50 | KHZ100 | KHZ200
*RST Setting: Depends upon the filter:
30 kHz filter: KHZ10
1 MHz filter: KHZ200
Test Set Requirements: E6601A WCTS Program Version A.05 and above
Example:
' Set the frequency spacing between measurements for the 30 kHz and 1 MHz filters to 5 kHz and 100 kHz respectively.
TestSet.WriteString("SETup:TDPChannel:SEMask:FREQuency:SPACing KHZ5, KHZ100")
Sets/queries the pass/fail limits for the following frequency offsets in the Spectrum Emission Mask measurement:
30 kHz filter ±0.8 MHz
30 kHz filter ±1.8 MHz
30 kHz filter ±2.4 MHz
1 MHz filter ±2.4 MHz
1 MHz filter ±4.0 MHz
Setting Range: -80 to 10 dBc
Query Range: -80 to 10 dBc
Resolution: 0.01 dBc
*RST Setting:
30 kHz filter ±0.8 MHz: -35.0 dB
30 kHz filter ±1.8 MHz: -49.0 dB
30 kHz filter ±2.4 MHz: -59.2 dB
1 MHz filter ±2.4 MHz: -44.0 dB
1 MHz filter ±4.0 MHz: -44.0 dB
Test Set Requirements: E6601A WCTS Program Version A.05 and above
Example:
' Set the pass/fail limits for the frequency offsets in the SEM measurement.
TestSet.WriteString("SETup:TDPChannel:SEMask:LIMit -35DB, -49DB, -59DB, -44DB, -44DB")
Sets/queries the test tolerance level for the Spectrum Emission Mask measurement.
Setting Range: 0 to 100 dB
Query Range: 0 to 100 dB
Resolution: 0.01 dB
*RST Setting: 1.5 dB
Test Set Requirements: E6601A WCTS Program Version A.05 and above
Example:
' Set the test tolerance level for the Spectrum Emission Mask measurement to 2.5 dB.
TestSet.WriteString("SETup:TDPChannel:SEMask:TTOLerance 2.5DB")