Spectrum Emission Mask (SEM) Measurement Description

Last Updated: August 29, 2007

This topic describes the Spectrum Emission Mask measurement. Spectrum Emission Mask is a measurement in the Dedicated Physical Channel measurement suite.

How is a Spectrum Emission Mask Measurement Made?

SEM is a relative measurement of the out-of-channel emissions to the in-channel. The purpose for this test is to measure the excess emissions that would interfere to other channels or to other systems.

The UE conformance specifications in 3GPP TS 34.122, Section 5.5.2.1 defines a mask for out of channel emissions. This mask is defined relative to the in-channel power.

In-Channel Power

The in-channel power is measured after filtering the signal with a=0.22, Root-Raised Cosine (RRC) filter. This measurement result is identical to the RRC Filtered Mean Power measurement.

Note: The in-channel measurement automatically runs the RRC Filtered Mean Power measurement, so there is no need to run the RRC Filtered Mean Power measurement while you are running the SEM measurement.

Out-of-Channel Emission

The out-of-channel emissions are measured using a Gaussian filter with either in a 30 kHz or 1 MHz noise bandwidth. The out-of-channel power applies to frequencies that are between 0.8 and 4.0 MHz away from the center carrier frequency.

Spectrum Emission Mask Measurement Parameters

Spectrum Emission Mask is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Parameters for details of the parameters that apply to measurements in the suite.

Spectrum Emission Mask Measurement Limits

Spectrum Emission Mask is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Limits for details of the limits parameters that apply to measurements in the suite.

Spectrum Emission Mask Measurement Results

Integrity Indicator

This result provides the integrity indicator for the Dedicated Physical Channel measurement suite. Normal indicates that the measurement suite completed successfully without error and the result is accurate. For details of other integrity indicators, see Measurement Integrity Indicator.

SCPI command: FETCh:TDPChannel:INTegrity?

Spectrum Emission Mask Overall Pass/Fail

This result provides the overall pass/fail for the Spectrum Emission Mask measurement. If any out-of-channel frequency range does not comply with the standard, the entire mask fails.  

SCPI commands: FETCh:TDPChannel:SEMask[:BURSt[1]][:PARTial]?, FETCh:TDPChannel:SEMask[:BURSt[1]]:BAND[:ALL]?  

In-Channel Power

This result provides the in-channel power in dBm/1.28 MHz.

SCPI commands: FETCh:TDPChannel:SEMask[:BURSt[1]]:BAND[:ALL]?, FETCh:TDPChannel:SEMask[:BURSt[1]]:RANGe[:ALL]?

Frequency Range Results

The following results are provided for each of the three individual frequency ranges; pass/fail, relative power level, frequency offset of the largest mask error, and the margin of that error.

SCPI commands:FETCh:TDPChannel:SEMask[:BURSt[1]]:RANGe[:ALL]? , FETCh:TDPChannel:SEMask[:BURSt[1]]:RANGe:RANGe([1]|2|3)?

Lower Band Results

SCPI commands: FETCh:TDPChannel:SEMask[:BURSt[1]]:BAND:LOWer([1]|2|3)[:ALL]?, FETCh:TDPChannel:SEMask:BAND:LOWer([1]|2|3):POINts?

Upper Band Results

SCPI commands: FETCh:TDPChannel:SEMask[:BURSt[1]]:BAND:UPPer([1]|2|3)[:ALL]?, FETCh:TDPChannel:SEMask:BAND:UPPer([1]|2|3):POINts?

Number of Points Tested

This result provides the number of points tested for all bands in the spectrum emission mask measurement. This is the sum of all of the number of points calculated using the formulas for each band.

SCPI command: FETCh:TDPChannel:SEMask:BAND:POINts?

Spectrum Emission Mask Input Signal Requirements

Spectrum Emission Mask is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Input Signal Requirements for details of the input signal requirements that apply to all measurements in the suite.   

 

Related Topics