Last Updated: August 29, 2007
This topic includes:
The DL Channel setting specifies the downlink UTRA Absolute RF Channel Number (UARFCN). This determines at what frequency the test set's RF generator will transmit the downlink signal.
The relationship between UARFCN and downlink frequency is described in 3GPP TS 25.101 section 5.
Downlink Frequency and UARFCN, and DL Channel Range
|
Band |
DL to UL Frequency Separation (MHz) |
Center Frequency Range (MHz) |
UARFCN Equation |
UARFCN Range |
Applicable Test Set Uplink Channel Range |
|
I |
190 |
2112.4 - 2167.6 increment = 0.2 |
5 * (center freq in MHz) |
10562 - 10838 |
10562 - 10838 |
|
II |
80 |
1932.4 - 1987.6 increment = 0.2 |
5 * (center freq in MHz) |
9662 - 9938 |
9662 - 9938 |
|
1932.5 - 1987.5 increment = 5 |
5 * ((center freq in MHz) - 1850.1 MHz) |
412, 437, 462, 487, 512, 537, 562, 587, 612, 637, 662, 687 |
412, 437, 462, 487, 512, 537, 562, 587, 612, 637, 662, 687 | ||
|
III |
95 |
1807.4 - 1877.6 increment = 0.2 |
5 * ((center freq in MHz) - 1575 MHz) |
1162 - 1513 |
1162 - 1513 |
|
IV |
400 |
2112.4 - 2152.6 increment = 0.2 |
5 * ((center freq in MHz) - 1805 MHz) |
1537 - 1738 |
1537 - 1738 |
|
2112.5 - 2152.5 increment = 5 |
5 * ((center freq in MHz) - 1735.1 MHz) |
1887, 1912, 1937, 1962, 1987, 2012, 2037, 2062, 2087 |
1887, 1912, 1937, 1962, 1987, 2012, 2037, 2062, 2087 | ||
|
V |
45 |
871.4 - 891.6 increment = 0.2 |
5 * (center freq in MHz) |
4357 - 4458 |
4357 - 4458 |
|
871.5, 872.5, 876.5, 877.5, 882.5, 887.5 |
5 * ((center freq in MHz) - 670.1 MHz) |
1007, 1012, 1032, 1037, 1062, 1087 |
1007, 1012, 1032, 1037, 1062, 1087 | ||
|
VI |
45 |
877.4 - 882.6 increment = 0.2 |
5 * (center freq in MHz) |
4387 - 4413 |
4387 - 4413 |
|
877.5, 882.5 |
5 * ((center freq in MHz) - 670.1 MHz) |
1037, 1062 |
1037, 1062 | ||
|
VII |
120 |
2622.4 - 2687.6 increment = 0.2 |
5 * ((center freq in MHz) - 2175 MHz) |
2237 - 2563 |
2237 - 2563 |
|
2622.5 - 2687.5 increment = 5 |
5 * ((center freq in MHz) - 2105.1 MHz) |
2587, 2612, 2637, 2662, 2687, 2712, 2737, 2762, 2787, 2812, 2837, 2862, 2887, 2912 |
2587, 2612, 2637, 2662, 2687, 2712, 2737, 2762, 2787, 2812, 2837, 2862, 2887, 2912 | ||
|
VIII (UMTS 900) |
45 |
927.4 - 957.6 increment = 0.2 |
5 * ((center freq in MHz) - 340 MHz) |
2937 - 3088 |
2937 - 3088 |
|
IX |
95 |
1847.4 - 1877.4 increment = 0.2 |
5 * (center freq in MHz) |
9237 - 9387 |
9237 - 9387 |
|
X |
400 |
2112.4 - 2167.6 increment = 0.2 |
5 * ((center freq in MHz)-1490 MHz) |
3112 - 3388 |
3112 - 3388 |
|
2112.5 - 2167.5 increment = 5 |
5 * ((center freq in MHz)-1430.1 MHz) |
3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 |
3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 | ||
|
XI (UMTS 1500 MHz) |
48 |
1478.4 - 1498.4 increment = 0.2 |
5 * ((center freq in MHz)-736 MHz) |
3712 - 3812 |
3712 - 3812 |
The DPCH DL Channel setting sets the test set's RF Generator to a specific uplink UARFCN value. Alternatively, you can set the downlink frequency. The DPCH DL Channel setting is located on the RF Generator tab of the RF Control window.
On the front panel, under SCREENS, press the Main/Call key to display the RF Control window.
Select the RF Generator tab.
Set the Control Mode to Auto.
Set DPCH DL Channel to the desired value.
SCPI Command: TRANsceiver:CHANnel:DOWNlink:FDD
The RF Generator's Frequency setting sets the downlink frequency. Alternatively, you can set the DPCH DL Channel. The downlinik Frequency setting is located on the RF Generator tab of the RF Control window.
On the front panel, under SCREENS, press the Main/Call key to display the RF Control window.
Select the RF Generator tab.
Set the Control Mode to Manual.
Set Frequency to the desired value.
SCPI Command: RFGenerator:FREQuency:WCALibration