Last Updated: August 29, 2007
These commands return the mean power results from the dedicated physical channel (DPCH) measurement suite.
For more information on the conventions used in the programming examples click here.
Queries the DPCH measurement suite integrity, the pass/fail mean power result, and the average mean power.
Query Range:
Dedicated physical channel measurement suite integrity: See Measurement Integrity Indicator.
Mean power overall pass/fail result: 0 (pass), 1 (fail)
Average mean power: <nr3> in dBm and 9.91 E+37 (NAN)
Test Set Requirements: E6601A WCTS Program Version A.02 and above
Example:
' Query the DPCH measurement suite integrity, the pass/fail mean power result, and the average mean power.
TestSet.WriteString("FETCh:WDPChannel:MPOWer?")
Queries the DPCH measurement suite integrity, mean power's overall pass fail result, minimum mean power, maximum mean power, average mean power, and the standard deviation.
Query Range:
Dedicated physical channel measurement suite integrity: See Measurement Integrity Indicator.
Mean power overall pass/fail result: 0 (pass), 1 (fail)
Minimum mean power: <nr3> in dBm and 9.91 E+37 (NAN)
Maximum mean power: <nr3> in dBm and 9.91 E+37 (NAN)
Average mean power: <nr3> in dBm and 9.91 E+37 (NAN)
Standard deviation: <nr3> in dB and 9.91 E+37 (NAN)
Test Set Requirements: E6601A WCTS Program Version A.02 and above
Example:
' Query the DPCH measurement suite integrity, mean power's overall pass fail result,
' minimum mean power, maximum mean power, average mean power, and the standard deviation.
TestSet.WriteString("FETCh:WDPChannel:MPOWer:ALL?")