FETCh:WDPChannel:RRCPower?

Last Updated: August 29, 2007

These commands return the Root Raised Cosine (RRC) filtered mean power results from the Dedicated Physical Channel (DPCH) measurement suite.

For more information on the conventions used in the programming examples click here.

FETCh:WDPChannel:RRCPower[:PARTial]?  

Queries the DPCH measurement suite integrity, the RRC filtered mean power's overall pass fail result, and the average RRC filtered mean power.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the DPCH measurement suite integrity, the RRC filtered mean power's overall pass fail result,

' and the average RRC filtered mean power.   

TestSet.WriteString("FETCh:WDPChannel:RRCPower?")

FETCh:WDPChannel:RRCPower:ALL?

Queries the DPCH measurement suite integrity, RRC filtered mean power's overall pass fail result, minimum RRC filtered mean power, maximum RRC filtered mean power, average RRC filtered mean power, and the standard deviation.

Query Range:

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Queries the DPCH measurement suite integrity, RRC filtered mean power's overall pass fail result,

' minimum RRC filtered mean power, maximum RRC filtered mean power, average RRC filtered mean power,

' and the standard deviation.  

TestSet.WriteString("FETCh:WDPChannel:RRCPower:ALL?")