SETup:MEASurement

Last Updated: August 29, 2007

For more information on the conventions used in the programming examples click here.

SETup:MEASurement:TTOLerance[:SELected][?]
SETup:MEASurement:TTOLerance:WCALibration[?]

Sets/queries the Enable Test Tolerances parameter, which determines whether or not all test tolerance levels are applied to measurement pass/fail results for the measurements contained in the DPCH measurement suite.  

The optional [:SELected] keyword specifies that the setting or query applies to the currently selected application.

Setting Range: 0 | OFF | 1 | ON

Query Range: 0 | 1

*RST Setting: 0 | OFF

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Enable test tolerance levels.

TestSet.WriteString("SETup:MEASurement:TTOLerance:WCALibration ON")