SETup:WDPChannel Common Parameters

Last Updated: August 29, 2007

These commands allow you to set and query general settings associated with the Dedicated Physical Channel (DPCH) measurement suite.

For more information on the conventions used in the programming examples click here.

SETup:WDPChannel:CONTinuous[?]

Sets/queries the trigger state for the Dedicated Physical Channel measurement suite.  See Triggering of Measurements.

Setting Range: Single trigger mode = 0 | OFF, Continuous trigger mode = 1 | ON  

Query Range: 0 | 1

*RST Setting: 0 | OFF

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the measurement suite to single trigger mode.

TestSet.WriteString("SETup:WDPChannel:CONTinuous OFF")

SETup:WDPChannel:COUNt[:SNUMber][?]

The setting form of this command performs two functions: (1) sets the multi-measurement count for the Dedicated Physical Channel measurement suite (see SETup:WDPChannel:COUNt:NUMBer[?]) and (2) sets the multi-measurement count state to on (see SETup:WDPChannel:COUNt:STATe[?]).

The query form of this command returns the current Dedicated Physical Channel measurement suite multi-measurement count value.

Setting Range: 1 to 999

Query Range: 1 to 999

*RST Setting: 10

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the state to on and the multi-measurement count value to 100.

TestSet.WriteString("SETup:WDPChannel:COUNt 100")

SETup:WDPChannel:COUNt:NUMBer[?]

Sets/queries the multi-measurement count for the Dedicated Physical Channel measurement suite.

Setting Range: 1 to 999

Query Range: 1 to 999

Resolution: 1

*RST Setting: 10

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the multi-measurement count value to 5.

TestSet.WriteString("SETup:WDPChannel:COUNt:NUMBer 5")

SETup:WDPChannel:COUNt:STATe[?]

Sets/queries the Dedicated Physical Channel measurement suite, multi-measurement state.

Setting Range: 0 | OFF | 1 | ON

Query Range: 0 | 1

*RST Setting:  0 | OFF

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Turn on DPCH measurement suite multi-measurements.

TestSet.WriteString("SETup:WDPChannel:COUNt:STATe ON")

SETup:WDPChannel:INITiate[?]

Sets/queries the measurements to enable for the Dedicated Physical Channel measurement suite.

After you perform a full preset of the test set, switch applications, or restart the test set, you must either send this command or the INITiate:WDPChannel[:ON] command, with one or more parameters specifying the measurements you want the RF Channel measurement suite to perform. Otherwise, if you attempt to use the INITiate:WDPChannel[:ON] command without specifying any parameters, the following error message is reported:

“Operation rejection; Sub-measurements must be enabled using ‘SETup:WDPChannel:INITiate <args>’ or ‘INITiate:WDPChannel[:ON] <args>’ before ‘INITiate:WDPChannel[:ON] can be accepted.”

Specifying a value of NONE disables all measurements in the suite.

If this command or the INITiate:WDPChannel[:ON] command has not enabled measurements in the suite since a power up, preset, or an application switch, the query form of this command returns a value of UNKN (short for UNKNown). This value indicates that you have not explicitly set up the measurements to enable for the Dedicated Physical Channel measurement suite, so it is indeterminate which sub-measurements are enabled.

Setting Range: One or more of the following values, separated by commas:

Query Range: One or more of the following values, separated by commas:

*RST Setting: UNKN

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the Dedicated Physical Channel measurement suite to include Mean Power
' and Spectrum Emissions Mask sub-measurements.

TestSet.WriteString("SETup:WDPChannel:INITiate MPOW,SEM")

SETup:WDPChannel:INITiate:COUNt?

Queries the number of measurements enabled for the Dedicated Physical Channel measurement suite.

Setting Range: 1 to 8

Query Range: 1 to 8

*RST Setting: 9

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Query the number of sub-measurements enabled for the Dedicated Physical Channel measurement suite.

TestSet.WriteString("SETup:WDPChannel:INITiate:COUNt?'")

SETup:WDPChannel:TIMeout[:STIMe][?]

The setting form of this command performs two functions: (1) sets the measurement timeout value in seconds for the Dedicated Physical Channel measurement suite (see SETup:WDPChannel:TIMeout:TIME[?]) and (2) sets the measurement timeout state to on (see SETup:WDPChannel:TIMeout:STATe[?]).

The query form of this command returns the current Dedicated Physical Channel measurement suite timeout value.

The units (S|MS) are optional, if no units are specified then units default to S.

Setting Range: 0.1 to 999.9 s

Query Range: 0.1 to 999.9 s

Resolution: 0.01 s

*RST Setting: 10 s

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the measurement suite timeout to 20 seconds and set the timeout state to on.

TestSet.WriteString("SETup:WDPChannel:TIMeout 20S")

SETup:WDPChannel:TIMeout:STATe[?]

Sets/queries the DPCH measurement suite's timeout (see Measurement Timeouts) state.

Setting Range: 0 | OFF | 1 | ON

Query Range: 0 | 1

*RST Setting:  0 | OFF

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the timeout state to On.

TestSet.WriteString("SETup:WDPChannel:TIMeout:STATe ON")

SETup:WDPChannel:TIMeout:TIME[?]

Sets/queries the DPCH measurement suite's timeout (see Measurement Timeouts) setting to be used when the timeout state is set to ON.

Setting Range: 0.1 to 999.9 s

Query Range: 0.1 to 999.9 s

Resolution: 0.01 s

*RST Setting: 10 s

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the timeout to 5 seconds.

TestSet.WriteString("SETup:WDPChannel:TIMeout:TIME 5S")

SETup:WDPChannel:TRIGger:DELay[?]

Sets/queries the DPCH measurement suite's trigger delay setting. See Triggering of Measurements.

This setting can be used to delay the measurement suite's trigger in order to start a measurement suite during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed.

Setting Range: -10 to 10 milliseconds

Query Range: -10 to 10 milliseconds

Resolution: 0.0001 millisecond

*RST Setting: 0 seconds

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the trigger delay to 1 ms.

TestSet.WriteString("SETup:WDPChannel:TRIGger:DELay 1MS")

SETup:WDPChannel:TRIGger:SOURce[?]

Sets/queries the DPCH measurement suite's trigger source. See Triggering of Measurements.

Setting Range: ARB | IMMediate | EXTernal

Query Range: ARB | IMM | EXT

*RST Setting: IMM

Test Set Requirements: E6601A WCTS Program Version A.02 and above; A.04 added ARB

Example:

' Set the trigger source to Immediate.

TestSet.WriteString("SETup:WDPChannel:TRIGger:SOURce IMM")

SETup:WDPChannel:TSLot[?]

Sets/queries the timeslot to test for the Dedicated Physical Channel measurement suite.

Setting Range: 0 to 14

Query Range: 0 to 14

Resolution: 1

*RST Setting: 0

Test Set Requirements: E6601A WCTS Program Version A.02 and above

Example:

' Set the timeslot to 4.

TestSet.WriteString("SETup:WDPChannel:TSLot 4")