Last Updated: August 29, 2007
This topic includes:
The Uplink Channel setting specifies the uplink UTRA Absolute RF Channel Number (UARFCN). This automatically sets the test set's receiver to the expected UE transmit frequency.
The relationship between UARFCN and uplink frequency is described in 3GPP TS 25.101 section 5.
Uplink Frequency and UARFCN, and Uplink Channel Range
|
Band |
DL to UL Frequency Separation (MHz) |
Center Frequency Range (MHz) |
UARFCN Equation |
UARFCN Range |
Applicable Test Set Uplink Channel Range |
|
I |
190 |
1922.4 - 1977.6 increment = 0.2 |
5 * (center freq in MHz) |
9612 - 9888 |
9612 - 9888 |
|
II |
80 |
1852.4 - 1907.6 increment = 0.2 |
5 * (center freq in MHz) |
9262 - 9538 |
9262 - 9538 |
|
1852.5 - 1907.5 increment = 5 |
5 * ((center freq in MHz) - 1850.1 MHz) |
12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287 |
12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287 | ||
|
III |
95 |
1712.4 - 1782.6 increment = 0.2 |
5 * ((center freq in MHz) - 1525 MHz) |
937 - 1288 |
937 - 1288 |
|
IV |
400 |
1712.4 - 1752.6 increment = 0.2 |
5 * ((center freq in MHz) - 1450 MHz) |
1312 - 1513 |
1312 - 1513 |
|
1712.5 - 1752.5 increment = 5 |
5 * ((center freq in MHz) - 1380.1 MHz) |
1662, 1687, 1712, 1737, 1762, 1787, 1812, 1837, 1862 |
1662, 1687, 1712, 1737, 1762, 1787, 1812, 1837, 1862 | ||
|
V |
45 |
826.4 - 846.6 increment = 0.2 |
5 * (center freq in MHz) |
4132 - 4233 |
4132 - 4233 |
|
826.5, 827.5, 831.5, 832.5, 837.5, 842.5 |
5 * ((center freq in MHz) - 670.1 MHz) |
782, 787, 807, 812, 837, 862 |
782, 787, 807, 812, 837, 862 | ||
|
VI |
45 |
832.4 - 837.6 increment = 0.2 |
5 * (center freq in MHz) |
4162 - 4188 |
4162 - 4188 |
|
832.5, 837.5 |
5 * ((center freq in MHz) - 670.1 MHz) |
812, 837 |
812, 837 | ||
|
VII |
120 |
2502.4 - 2567.6 increment = 0.2 |
5 * ((center freq in MHz) - 2100 MHz) |
2012 - 2338 |
2012 - 2338 |
|
2502.5 - 2567.5 increment = 5 |
5 * ((center freq in MHz) - 2030.1 MHz) |
2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 |
2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 | ||
|
VIII (UMTS 900) |
45 |
882.4 - 912.6 |
5 * ((center freq in MHz) - 340 MHz) |
2712 - 2863 |
2712 - 2863 |
|
IX |
95 |
1752.4 - 1782.4 increment = 0.2 |
5 * (center freq in MHz) |
8762 - 8912 |
8762 - 8912 |
|
X |
400 |
1712.4 - 1767.6 increment = 0.2 |
5 * ((center freq in MHz)-1135 MHz) |
2887 - 3163 |
3112 - 3388 |
|
1712.5 - 1767.5 increment = 5 |
5 * ((center freq in MHz)-1075.1 MHz) |
3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 |
3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 | ||
|
XI (UMTS 1500) |
48 |
1430.4 - 1450.4 increment = 0.2 |
5 * ((center freq in MHz)-733 MHz) |
3487 - 3587 |
3487 - 3587 |
This parameter directly sets the Uplink Channel setting to a specific uplink UARFCN value.
The Uplink Channel setting is located on the RF Analyzer tab of the RF Control window. To change this via the front panel:
On the front panel, under SCREENS, press the Main/Call key to display the RF Control window.
Select the RF Analyzer tab.
Set the Control Mode to Manual
Set Manual Mode to Channel.
Set Uplink Channel to the desired value.
SCPI Command: RFANalyzer:MANual:CHANnel:WCALibration
When Control Mode is set to Auto, the uplink UARFCN is automatically determined by the Uplink Channel Separation setting (the test set subtracts the frequency separation associated with the DL Channel's band from the DPCH DL Channel setting).
To set the RF Analyzer Control Mode to Auto:
Press the Main/Call key to display the RF Control window.
Select the RF Generator tab.
Set the correct DTCH DL Channel or Frequency (depending on the Control Mode setting).
Select the RF Analyzer tab.
Set the Control Mode to Auto
Set the Uplink Channel Separation.
SCPI command: RFANalyzer:CONTrol:FREQuency:AUTO:WCALibration