Operation

Overview

The M9379A consists of the following components.

The specification of each component is described in the data sheet.

Soft Front Panel

Power supply to Amplifiers and Switches: Master switch for amplifiers both 1 and 2 and switches.

LED on the front panel is changed as follows.

Amplifier 1

Switch

Furnished Cables

The two semi-rigid cables are furnished with the M9379A. The example of connections are shown below.