Corrections/De-embedding

This capability requires license model N7653APPC.

This topic describes the RF Output > Corrections/De-embedding screen, where you can configure and apply external corrections for your test setup.

Overview

Corrections On

Center Frequency Corrections Only

Add from Measurement

Configure Sensor ClosedSetup

Power Measurement Device

Start Frequency

Stop Frequency

Number of Steps

Power Meter Properties ClosedSetup

Power Meter Connection Type

Power Meter IP Address

Power Meter VXI-11 Device Name

Power Meter HiSLIP Device Name

Power Meter USB Device Name

Power Meter USB Device Name List

Power Meter IP Port

Power Meter Calibrate Sensor

Power Meter Calibrate Sensor from the Device List

Power Meter Zero Sensor

Power Meter Zero Sensor from the Device List

Spectrum Analyzer Properties ClosedSetup

Spectrum Analyzer Connection Type

Spectrum Analyzer Hostname or IP Address

Spectrum Analyzer VXI-11 Device Name

Spectrum Analyzer HiSlip Address

Spectrum Analyzer USB Device Name

Spectrum Analyzer IP Port

Spectrum Analyzer USB Device Name List

Measure Correction Data

Abort

Block Properties ClosedSetup

Count

Add from File

Clear

Delete Block

Move Left or Move Right

Enable

File

De-embed/embed

Reverse Ports

Snn = 0

Absolute Power Table Preset

Absolute Power Table Pair

Absolute Power Table Points

Absolute Power Table Frequency

Absolute Power Table Store

Absolute Power Table Initialize Frequency Step

Channel to Channel (C2C) Corrections and Channel Flatness Refresh ClosedSetup

Hold the Hardware State

Hold the Flatness Correction

Retrieve Usable Bandwidth

Retrieve Hardware PathID for Current State

Retrieve Hardware PathID for Frequency and Mode

Retrieve Hardware PathIDs for Mode

Set Hardware Path

Enable Hardware Path

Retrieve Hardware Band Transition Frequencies

Offset Channel Level Flatness Data

Clear Channel Level Flatness Data Offsets

Set I/Q Delay Offset

Clear I/Q Delay Offset

Set Phase Accumulator Delay Offset

Clear Phase Accumulator Delay Offset

Set Phase Offset

Clear Phase Offset

Set Measured Baseband Delay

Clear Measured Baseband Delay

Update Quiescent Temperature

Retrieve Fundamental Frequency

Retrieve Frequency Translation Type

Overview

The instrument has the capability to extend the Reference Plane beyond the factory calibrated RF Output port. The Reference Plane can be extended via Corrections and/or S-parameter de-embedding.

Up to four stages of correction and de-embedding are available. These stages are referred to as blocks and are labeled as Block A, B, C, and D. For SCPI commands, block A=1, B=2, and so on.

The following table lists the available correction and de-embedding components for your test setup.

Component Purpose Supported File Format(s)
Factory Cal

Directly measured correction data created during the factory manufacturing process or annual calibration.

N/A
Block A

User correction data applied on top of the Factory Cal.

For this block, you can:

  • either apply corrections from a specified correction file.

  • or measure directly with a supported power meter, spectrum analyzer, or network analyzer to generate a correction file.

.csv

.uflat (for compatibility with other Keysight Technologies signal generators)

Block B

De-embedding of fixtures including cables, connectors, and other passive components between the instrument and DUT to remove the effects of these test fixtures from the measurement results.

Individual fixture blocks represent different fixture elements in your test setup.

Calculated correction data for the sum of Blocks B, C, and/or D is applied on top of the Block A and/or Factory Cal.

Prior to the software version A.14.00, only the S21 data of the fixture was used for correction. With software version A.14.00 or later, the S11 and S21 data of the fixture are used for correction. Due to this difference in the S-parameters used for correction in these software versions, the calculated correction data may vary for these software versions.
.s2p
Block C
Block D

Configuring and applying user correction data using Block A

Adding fixture blocks (Block B, C, or D) for de-embedding

 

 

Corrections On

Enables or disables the user-flatness corrections.

GUI Location

RF Output > Corrections/De-embedding > Corrections On

SCPI Command

[:SOURce][:RF<channel>]:CORRection[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection[:STATe]?

SCPI Example

CORR ON

CORR?

Notes Output power may become too high when Corrections/Deembedding fixture's S-parameter includes S21 = 0.

Preset

0

State Saved

Yes

Backwards Compatibility SCPI

N51XXB:

[:SOURce]:CORRection[:STATe]

Backwards Compatibility Notes

For N51xxB:

Expand [:SOURce]:CORRection[:STATe] to [:SOURce][:RF<channel>]:CORRection[:STATe]

Initial S/W Revision

A.01.00

Center Frequency Corrections Only

Ignores the complex response data in measured (block A) or s2p (block B, C, D) data and only applies the absolute power, phase and time corrections.

GUI Location

RF Output > Corrections/De-embedding > Center Frequency Correction Only

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CFConly[1]|2[:STATe] ON|OFF|0|1

[:SOURce][:RF<channel>]:CORRection:CFConly[1]|2[:STATe]?

SCPI Example

For Block A:

CORR:CFC ON

CORR:CFC?

For Block B, C, D

CORR:CFC2 ON

CORR:CFC2?

Preset

0

State Saved

Yes

Backwards Compatibility SCPI

[:SOURce][:RF<channel>]:CORRection:APConly[:STATe]

Backwards Compatibility Notes

Alias [:SOURce][:RF<channel>]:CORRection:APConly[:STATe] to

[:SOURce][:RF<channel>]:CORRection:CFConly[1][:STATe];

[:SOURce][:RF<channel>]:CORRection:CFConly2[:STATe]

Initial S/W Revision

A.02.00

Modified S/W Revision

A.19.01 - Changed from "applies to both measured and s2p data" to "applies to measured or s2p data".

Add from Measurement

You can use the Block A properties > Add from Measurement button to access the Measure Corrections wizard. Using this wizard, you can configure and run the user correction measurement. The correction data generated from this measurement is saved to a .csv file. This file is then used as the correction file.

The subsections below describe the SCPI commands available to configure and run the user correction measurement.

Configure Sensor

SCPI commands defined in this section can be used to set up Correction measurements and Power Sensors used. In the user interface, these settings are included in the RF Output block's, Corrections/De-embedding block setup, when the Add from Measurement button is selected.

Supported measurement devices are as follows.

Keysight U8480 Series USB Thermocouple Power Sensor

Keysight U2000 Series USB Sensors

Including:

U2000 Series USB Power Sensors:

X-Series Signal Analyzers:

Use Device List

Enables the Device List to be the sole method of specifying a Spectrum Analyzer or Power Meter to be used for Correction Measurement.

To configure external devices in the Device List, see Device List.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device > Use Device List (checkbox)

SCPI Command

[:SOURce][:RF<channel>]:CORRection:DLISt ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:DLISt?

SCPI Example

RF3:CORR:DLIS ON

RF3:CORR:DLIS?

Preset

This is unaffected by a Preset but is set to OFF on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Choices

ON | OFF | 1 | 0

Initial S/W Revision

A.12.00

Specify Device for Correction Measurement

Specifies a Power Meter or a Spectrum Analyzer from the Device List for user Correction Measurement. Note that the reference clock must be locked between the signal generator and Spectrum Analyzers.

To configure external devices in the Device List, see Device List.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device > Use Device List (selected) > Configure Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:DEVice <name>

[:SOURce][:RF<channel>]:CORRection:DEVice?

SCPI Example

RF3:CORR:DEV "myDevice"

RF3:CORR:DEV?

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Spectrum Analyzer or Power Meter, an error will be raised:

-220,"Parameter error; Correction Measurement requires a Spectrum Analyzer or Power Meter device type"

Couplings

If the device currently selected from the Device List is removed, this setting will default to NONE

Value will only be utilized by hardware when Use Device List for Correction Measurement is set to ON.

Preset

This is unaffected by a Preset but is set to an empty string on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Initial S/W Revision

A.12.00

Power Measurement Device

Selects the hardware type used in the user correction measurement when the Device List is not being used.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMDevice PMETer|SANalyzer

[:SOURce][:RF<channel>]:CORRection:PMDevice?

SCPI Example

CORR:PMD PMET

CORR:PMD?

Couplings

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

PMETer

State Saved

Yes

Choices

Power Meter | Spectrum Analyzer

Initial S/W Revision

A.01.00

Modified S/W Revision

A.12.00

Start Frequency

Sets the start frequency for the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Start Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STARt <freq>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STARt?

SCPI Example

CORR:FLAT:STEP:STAR 1GHz

CORR:FLAT:STEP:STAR?

Couplings

Coupled to Stop Frequency. If Start Frequency goes above Stop Frequency, Stop Frequency is automatically adjusted to Start Frequency.

Preset

1 GHz

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: Max

State Saved

Yes

Min

9 kHz

Max

For M9484C:

  • With Option 506: 6 GHz

  • With Option 508: 8.5 GHz

  • With Option 514: 14 GHz

  • With Option 520: 21.6 GHz

  • With Option 532: 31.8 GHz

  • With Option 544: 44 GHz

  • With Option 554: 54 GHz

  • With Option AL2 and V3080A-F06 connected: 67 GHz

  • With Option AL2 and V3080A-F07 connected: 75 GHz

  • With Option AL2 and V3080A-F09 connected: 90 GHz

  • With Option AL2 and V3080A-F11 connected: 110 GHz

Resolution

0. 00001 Hz

Initial S/W Revision

A.01.00

Modified S/W Revision

A.09.00, A.11.00

History

Added M9484C at A.09.00

Added M9484C-AL2 and V3080A at A.11.00

Stop Frequency

Sets the stop frequency for the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Stop Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STOP <freq>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STOP?

SCPI Example

CORR:FLAT:STEP:STOP 1GHz

CORR:FLAT:STEP:STOP?

Couplings

Coupled to Start Frequency. If Stop Frequency goes below Start Frequency, Start Frequency is automatically adjusted to Stop Frequency.

Preset

2 GHz

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: Max

State Saved

Yes

Min

9 kHz

Max

For M9484C:

  • With Option 506: 6 GHz

  • With Option 508: 8.5 GHz

  • With Option 514: 14 GHz

  • With Option 520: 21.6 GHz

  • With Option 532: 31.8 GHz

  • With Option 544: 44 GHz

  • With Option 554: 54 GHz

  • With Option AL2 and V3080A-F06 connected: 67 GHz

  • With Option AL2 and V3080A-F07 connected: 75 GHz

  • With Option AL2 and V3080A-F09 connected: 90 GHz

  • With Option AL2 and V3080A-F11 connected: 110 GHz

Resolution

0.00001 Hz

Initial S/W Revision

A.01.00

Modified S/W Revision

A.09.00, A.11.00

History

Added M9484C at A.09.00

Added M9484C-AL2 and V3080A at A.11.00

Number of Steps

Defines the number of points in the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Number of Steps

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:POINts <integer>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP: POINts?

SCPI Example

CORR:FLAT:STEP:POIN 2

CORR:FLAT:STEP:POIN?

Preset

10

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: 2

State Saved

Yes

Min

2

Max

10000

Initial S/W Revision

A.01.00

Power Meter Properties

Sets the power meter properties when Power Meter is the selected Power Measurement Device.

Power Meter Connection Type

Sets the type of control connection for communication using the external power meter for corrections calibration.

VXI11

Enables the power meter for VXI-11 control through the signal generator. A power meter with GPIB can be controlled through VXI-11 using a LAN-GPIB gateway.

HISLip

Enables the power meter for HiSlip control through the signal generator

SOCKets

Enables the power meter for sockets LAN control through the signal generator.

USB

Enables the power meter for USB control through the signal generator.

Initial S/W Revision

A.01.00

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN, (Instrument VXI-11, HiSLIP, Socket) or USB

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:TYPE SOCKets|VXI11|USB|HISLip

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:TYPE?

SCPI Example

CORR:PMET:COMM:TYPE SOCK

CORR:PMET:COMM:TYPE?

Notes

The settings enabled by this command are not affected by a signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

SOCKets

State Saved

No

Choices

Socket | VXI11 | USB | HiSlip

Initial S/W Revision

A.01.00

Power Meter IP Address

Sets the internet protocol (IP) address for a power meter that is controlled by the signal generator for corrections calibration. If connecting to a GPIB power meter through a LAN-GPIB gateway, this command sets the IP address of the gateway.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > Connection Type LAN > Set LAN IP Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:IP <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:IP?

SCPI Example

CORR:PMET:COMM:LAN:IP "192.168.1.5"

CORR:PMET:COMM:LAN:IP?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST. Ensure that the power meter IP address is different from the signal generator address.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Initial S/W Revision

A.01.00

Power Meter VXI-11 Device Name

Specifies the VXI-11 device name for a power meter that is being controlled by the signal generator for corrections calibration. If connecting directly to the power meter, enter the name as specified on your power meter documentation. If connecting through a LAN-GPIB gateway, enter the SICL address of the power meter.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Instrument (VXI-11) > Remote Name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:DEVice?

SCPI Example

CORR:PMET:COMM:LAN:DEV "instr0"

CORR:PMET:COMM:LAN:DEV?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

inst0

State Saved

No

Initial S/W Revision

A.01.00

Power Meter HiSLIP Device Name

Specifies the HiSLIP device name for a power meter that is being controlled by the signal generator for corrections calibration. If connecting directly to the power meter, enter the name as specified in your power meter documentation.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type LAN > HiSLIP > Remote Name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:HISLip:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:HISLip:DEVice?

SCPI Example

CORR:PMET:COMM:HISL:DEV "hslip1"

CORR:PMET:COMM:HISL:DEV?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

hislip0

State Saved

No

Initial S/W Revision

A.01.00

Power Meter USB Device Name

Selects the USB device to be used for corrections calibration. The query returns the USB device identification.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type USB > Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:DEVice?

SCPI Example

CORR:PMET:COMM:USB:DEV "instr0"

CORR:PMET:COMM:USB:DEV?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Initial S/W Revision

A.01.00

Power Meter USB Device Name List

Remote command only.

Returns a listing of all connected USB devices.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:LIST?

SCPI Example

CORR:PMET:COMM:USB:LIST?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

State Saved

No

Initial S/W Revision

A.01.00

Power Meter IP Port

Sets the IP port number on the power meter that is controlled by the signal generator for corrections calibration.

5025

Standard mode. The command enables standard mode for simple programming.

5024

Telnet mode. The command enables the telnet SCPI service for programming.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type LAN > Protocol set to Socket > Port Number

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:PORT <integer>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:PORT?

SCPI Example

CORR:PMET:COMM:LAN:PORT 5025

CORR:PMET:COMM:LAN:PORT?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

5025

State Saved

No

Initial S/W Revision

A.01.00

Power Meter Calibrate Sensor

Calibrates the connected power meter. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Calibrate Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:CALibrate

SCPI Example

CORR:PMET:CAL

Initial S/W Revision

A.01.00

Power Meter Calibrate Sensor from the Device List

Calibrates the connected power meter from the Device List. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Use Device List (checked) > Configure Device > (select or add a device) > Calibrate Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:CALibrate:DLISt <string>

SCPI Example

CORR:PMET:CAL:DLIS "myDevice"

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Power Meter, an error will be raised:

-220,"Parameter error; Power Meter Calibrate Sensor requires a Power Meter device type"

Initial S/W Revision

A.12.00

Power Meter Zero Sensor

Zeroes the connected power meter. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Zero Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:ZERO

SCPI Example

CORR:PMET:ZERO

Initial S/W Revision

A.01.00

Power Meter Zero Sensor from the Device List

Zeroes the connected power meter from the Device List. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Use Device List (checked) > Configure Device > (select or add a device) > Zero Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:ZERO:DLISt <string>

SCPI Example

CORR:PMET:ZERO:DLIS "myDevice"

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Power Meter, an error will be raised:

-220,"Parameter error; Power Meter Zero Sensor requires a Power Meter device type"

Initial S/W Revision

A.12.00

Spectrum Analyzer Properties

Sets the spectrum analyzer properties when Spectrum Analyzer is the selected Power Measurement Device.

Spectrum Analyzer Connection Type

Sets the type of control connection for communication with the external spectrum analyzer for corrections calibration.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN, (Instrument VXI-11, HiSLIP, Socket) or USB

VXI11

Enables the spectrum analyzer for VXI-11 control through the signal generator. A spectrum analyzer with GPIB can be controlled through VXI-11 using a LAN-GPIB gateway.

HISLip

Enables the spectrum analyzer for HiSlip control through the signal generator.

SOCKets

Enables the spectrum analyzer for sockets LAN control through the signal generator.

USB

Enables the spectrum analyzer for USB control through the signal generator.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:TYPE SOCKets |VXI11|USB|HISLip

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:TYPE?

SCPI Example

CORR:SAN:COMM:TYPE SOCK

CORR:SAN:COMM:TYPE?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

SOCKets

State Saved

No

Choices

Socket | VXI11 | USB | HiSlip

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:TYPE

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:TYPE to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:TYPE

Initial S/W Revision

A.01.00

Modified at S/W Revision A.20.00 - Added N51xxB Backwards Compatibility
Spectrum Analyzer Hostname or IP Address

Sets the internet protocol (IP) address for a spectrum analyzer that is controlled by the signal generator for corrections calibration. If connecting to a GPIB spectrum analyzer through a LAN-GPIB gateway, this command sets the IP address of the gateway.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Hostname or IP Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:IP <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:IP?

SCPI Example

CORR:SAN:COMM:LAN:IP "192.168.1.5"

CORR:SAN:COMM:LAN:IP?

Notes

  • The setting enabled by this command is not affected by signal generator power-on, preset, or *RST. Ensure that the spectrum analyzer IP address is different from the signal generator address.

  • Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:LAN:IP

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:LAN:IP to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:LAN:IP

Initial S/W Revision

A.01.00

Modified at S/W Revision A.20.00 - Added N51xxB Backwards Compatibility
Spectrum Analyzer VXI-11 Device Name

Enter a VXI-11 device name for a spectrum analyzer that is being controlled by the signal generator for corrections calibration. If connecting directly to the spectrum analyzer, enter the name as specified on your spectrum analyzer documentation. If connecting through a LAN-GPIB gateway, enter the SICL address of the spectrum analyzer.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Instrument (VXI-11) > Remote Name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:DEVice?

SCPI Example

CORR:SAN:COMM:LAN:DEV "instr0"

CORR:SAN:COMM:LAN:DEV?

Notes

  • The setting enabled by this command is not affected by a signal generator power-on, preset, or *RST.

  • Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

inst0

State Saved

No

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:LAN:DEVice

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:LAN:DEVice to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:LAN:DEVice

Initial S/W Revision

A.01.00

Modified at S/W Revision A.20.00 - Added N51xxB Backwards Compatibility
Spectrum Analyzer HiSlip Address

Enter a HiSlip device name for a spectrum analyzer that is being controlled by the signal generator for corrections calibration. If connecting directly to the spectrum analyzer, enter the name as specified on your spectrum analyzer documentation.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > HiSLIP > Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:HISLip:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:HISLip:DEVice?

SCPI Example

CORR:SAN:COMM:HISL:DEV "instr0"

CORR:SAN:COMM:HISL:DEV?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

hislip0

State Saved

No

Initial S/W Revision

A.01.00

Spectrum Analyzer USB Device Name

Selects the USB device to be used for corrections calibration. The query returns the USB device identification.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > USB > Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:DEVice?

SCPI Example

CORR:SAN:COMM:USB:DEV "instr0"

CORR:SAN:COMM:USB:DEV?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Initial S/W Revision

A.01.00

Spectrum Analyzer IP Port

Sets the spectrum analyzer's IP port number that is controlled by the signal generator for corrections calibration.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Protocol set to Socket > Port

5025

Standard mode. The command enables standard mode for simple programming.

5024

Telnet mode. The command enables the telnet SCPI service for programming.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:PORT <integer>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:PORT?

SCPI Example

CORR:SAN:COMM:LAN:PORT 5025

CORR:SAN:COMM:LAN:PORT?

Notes

  • The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

  • Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

5025

State Saved

No

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:LAN:PORT

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:LAN:PORT to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:LAN:PORT

Initial S/W Revision

A.01.00

Modified at S/W Revision A.20.00 - Added N51xxB Backwards Compatibility
Spectrum Analyzer USB Device Name List

Remote command only.

Query only. Returns a listing of all connected USB devices.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:LIST?

SCPI Example

CORR:SAN:COMM:USB:LIST?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

State Saved

No

Initial S/W Revision

A.01.00

Measure Correction Data

The measured correction data will be saved to the specified file. The file path can be either a full or a relative path. When a relative path is given as file path, it will be based from:

<Documents>\Keysight\PathWave\SignalGenerator\Corrections

If no file is specified, a file name is automatically created.

This is an overlapped command that initiates the Correction Data measurement. The measurement can be aborted by the Abort command.

Note that the reference clock must be locked between the signal generator and the spectrum analyzer.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Measure Corrections > Measure Correction Data

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:CALibrate [<file_name>]

SCPI Example

CORR:FLAT:CAL

State Saved

No

Initial S/W Revision

A.01.00

Abort

Aborts the Correction Data measurement.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Measure Corrections > Abort

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:CALibrate:ABORt

SCPI Example

CORR:FLAT:CAL:ABOR

State Saved

No

Initial S/W Revision

A.01.00

Block Properties

There can be up to four blocks in Corrections Setup. These blocks belong to the following two types.

To access Block Properties from the GUI, click on the applicable Block- Block A, Block B, Block C or Block D.

Count

Displays or returns the number of Blocks configured for corrections. The maximum number of blocks is four. The minimum number is 1. The first block is for User Corrections and is always present.

GUI Location

RF Output > Corrections/De-embedding

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:COUNt?

SCPI Example

CORR:BLOC:COUN?

Initial S/W Revision

A.01.00

Add from File

Adds a fixture block at the end of blocks.

GUI Location

RF Output > Corrections/De-embedding > Add from File

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:ADD:FIXTure [<file_name>[,<apply>[,<rport>]]]

SCPI Example

CORR:BLOC:ADD:FIXT "data.s2p"

Notes

Attempting to send a SCPI without <file_name> raises the error -109, "Missing parameter". <apply> and <rport> can be omitted.

State Saved

No

Initial S/W Revision

A.01.00

Clear

Remote command only.

Clears all the blocks except for the first one. The first block is for User Correction and cannot be deleted from the list.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:CLEar:FIXTure

SCPI Example

CORR:BLOC:CLE:FIXT

Initial S/W Revision

A.01.00

Delete Block

Deletes the specified block. If the specified block doesn’t exist, it issues an error.

There is no SCPI command for this function.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Delete Block

Initial S/W Revision

A.01.00

Move Left or Move Right

Moves the specified block to the specified position. If the specified block doesn’t exist, it issues an error. If the destination block is smaller than the number of blocks, it issues an error.

There is no SCPI command for this function.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Move Left or Move Right

Initial S/W Revision

A.01.00

File

Sets or queries the correction data file (.csv or .uflat) for Block A and .s2p file for Block B, C, or D.

The default folder location is:

<Documents>\Keysight\PathWave\SignalGenerator\Corrections

File format for Block A

For Block A (1 in SCPI), the file can be a .uflat file compatible with other Keysight Technologies signal generators, or a .csv file.

The .csv file must be formatted as follows:

<Frequency in Hz>,<Amplitude in dB>,<Phase in radian>

For M9484C with N7653APPC subscription date of June 1, 2024 or later, the following two formats are supported for Block A .csv file:

Frequency,Amplitude,Phase,Time format .csv file

<Frequency in Hz>,<Amplitude in dB>,<Phase in radian>,<Time in seconds>

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Change File, current file name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk[1]|2|3|4:FILE <file_name>

[:SOURce][:RF<channel>]:CORRection:BLOCk[1]|2|3|4:FILE?

SCPI Example

CORR:BLOC:FILE "FixtureChannel2"

Notes

Attempting to load a Block A .csv file with four elements in a row, without N7653APPC of subscription date of June 1, 2024 or later, raises the error +703, Feature not supported; N7653APPC with subscription date June 1, 2024, is required.

Attempting to load a Block A .csv file with four elements in a row, on an unsupported instrument will raise the error +703, Feature not supported; Correction file cannot contain four elements on {Model}.

Preset

""

State Saved

Yes

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:CORRection:FLATness:LOAD

Backwards Compatibility Notes

For N51xxB:

  • Alias [:SOURce]:CORRection:FLATness:LOAD to [:SOURce]:RF1:CORRection:BLOCk1:FILE

  • .userflat is appended to the filename.

  • Alias [:SOURce][:RF<channel>]:CORRection:FLATness:LOAD to [:SOURce][:RF<channel>]:CORRection:BLOCk1:FILE

  • The aliased command applies to Block 1/A only.

Initial S/W Revision

A.01.00

Modified S/W Revision

A.15.00 - M9484C with N7653APPC subscription date of June 1, 2024 permitted BLOCk1 to accept User Correction of Frequency,Amplitude,Phase,Time .csv file.

A.20.00 - Added :CORRection:FLATness:LOAD as an alias for Block 1/A

Enable

Enables or disables the selected block.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Enable

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{1:4}[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk{1:4}[:STATe]?

SCPI Example

CORR:BLOC 1

CORR:BLOC?

State Saved

Yes

Initial S/W Revision

A.01.00

De-embed/embed

Specifies how the data is applied to the cascaded correction data. When De-embed is selected, the output at the frequency point is adjusted to compensate for the amplitude and phase changes introduced by the block. When Embed is selected, it is adjusted to include them.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Deembed or Embed

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:APPLy DEEMbedding|EMBedding
[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:APPLy?

SCPI Example

CORR:BLOC2:APPL EMB

CORR:BLOC2:APPL?

State Saved

Yes

Choices

De-embed | Embed

Initial S/W Revision

A.01.00

Reverse Ports

Specifies whether the port is reversed or not.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Reverse Ports

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:RPORt ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:RPORt?

SCPI Example

CORR:BLOC2:RPOR 1

CORR:BLOC2:RPOR?

State Saved

Yes

Initial S/W Revision

A.01.00

Snn = 0

Enables or disables Snn = 0.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Snn = 0

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk2|3|4:REFLection:ZERO ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk2|3|4:REFLection:ZERO?

SCPI Example

CORR:BLOC2:REFL:ZERO 1

CORR:BLOC2:REFL:ZERO?

Preset OFF

State Saved

Yes

Initial S/W Revision

A.18.00

Absolute Power Table Preset

Remote command only.

Initializes the Absolute Power table to a single point at the maximum frequency of the instrument with 0 dB correction.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:PRESet

SCPI Example

CORR:FLAT:PRES

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:PRESet

Backwards Compatibility Notes

For N51xxB:

Expand [:SOURce]:CORRection:FLATness:PRESet to [:SOURce][:RF<channel>]:CORRection:FLATness:PRESet
Initial S/W Revision A.20.00

Absolute Power Table Pair

Remote command only.

Inserts or updates a frequency/amplitude pair in the Absolute Power table.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:PAIR <freq>,<amplitude>

SCPI Example

CORR:FLAT:PAIR 1E9,-1.5

Notes The table is kept sorted by ascending frequency. The max pairs in the table are 3201.
State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:PAIR

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:PAIR to [:SOURce][:RF<channel>]:CORRection:FLATness:PAIR
Initial S/W Revision A.20.00

Absolute Power Table Points

Remote command only.

Returns the number of frequency/amplitude pairs currently in the Absolute Power table.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:POINts?

SCPI Example

CORR:FLAT:POIN?

State Saved No
Min 0
Max 3201
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:POINts?

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:POINts? to [:SOURce][:RF<channel>]:CORRection:FLATness:POINts?
Initial S/W Revision A.20.00

Absolute Power Table Frequency

Remote command only.

Query only command. Returns the frequency (in Hz) of the specified point in the Absolute Power table . <point> is a 1-based integer index.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:FREQuency? <point>

SCPI Example

CORR:FLAT:FREQ? 1

Notes If <point> is less than 1 or greater than the number of points in the table, raises error -224,"Illegal parameter value;Point index out of range."
State Saved No
Min 1
Max 3201
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:FREQuency?

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:FREQuency? to [:SOURce][:RF<channel>]:CORRection:FLATness:FREQuency?
Initial S/W Revision A.20.00

Absolute Power Table Store

Remote command only.

Saves the current in-memory Absolute Power table to a file in the Corrections directory.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STORe <"file">

SCPI Example

CORR:FLAT:STOR "myfile.csv"

CORR:FLAT:STOR "myfile.uflat"

CORR:FLAT:STOR "myfile.userflat"

CORR:FLAT:STOR "myfile"

Notes
  • The file format is determined by the file extension: .csv for CSV format, .uflat or .userflat for compatibility.

  • When no extension is provided and SCPI Backwards Compatibility Mode is set to N51xxB, .userflat is automatically appended to the filename. In all other modes, the file is saved in CSV format without an extension.

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:STORe

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:STORe to [:SOURce][:RF<channel>]:CORRection:FLATness:STORe
Initial S/W Revision A.20.00

Absolute Power Table Initialize Frequency Step

Remote command only.

Initializes the Absolute Power table with linearly spaced frequencies from Start Frequency to Stop Frequency using the configured Number of Steps. All amplitudes are set to 0 dB.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:INITialize:FSTep

SCPI Example

:CORRection:FLATness:INITialize:FSTep

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:INITialize:FSTep

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:INITialize:FSTep to [:SOURce][:RF<channel>]:CORRection:FLATness:INITialize:FSTep
Initial S/W Revision A.20.00

Channel to Channel (C2C) Corrections and Channel Flatness Refresh

For M9484C, the N7653APPC subscription date of June 1, 2024 or later is required to apply specific aspects of C2C.

By extending the reference plane for flatness performance beyond the front panel to some other connection point, band breaks that exist in the hardware can be handled optimally, improving residual instrument deviations.

Applying correction via correction de-embedding blocks A and B is preferable. Optimal results will result from leveraging of those corrections with these correction de-embedding blocks. See Corrections/De-embedding Overview.
Run Alignments immediately before doing any Channel to Channel Correction and keep temperature constant .

Hold the Hardware State

For M9484C

Remote command only.

Locks the hardware in the current state. The command is expected to be used to measure correction factors in overlap regions of the hardware block diagram.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:LOCK ON|OFF|1|0

[:SOURce][:RF<channel>]:HARDware:LOCK?

SCPI Example

:HARD:LOCK ON

:HARD:LOCK?

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.15.00

Hold the Flatness Correction

For M9484C

Remote command only.

Locks the flatness correction at the center frequency at the current conditions.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:FCFValue :LOCK ON|OFF|1|0

[:SOURce][:RF<channel>]:HARDware:FCFValue:LOCK?

SCPI Example

:HARD:FCFV:LOCK ON

:HARD:FCFV:LOCK?

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.15.00

Retrieve Usable Bandwidth

For M9484C

Remote command only.

Query only command.

Returns lower bound and upper bound frequencies for the provided PathID and dB threshold.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:UBANdwidth? <integer_pathId>,<float_threshold>

SCPI Example

:HARD:UBAN? 50,3.1 ! PathId=50, dB=3.1

Notes <float_threshold> is a floating point value for dB to 0.1 dB resolution. The return values are two integers of frequency with 1 Hz resolution.

State Saved

No

Initial S/W Revision

A.15.00

Retrieve Hardware PathID for Current State

For M9484C

Remote command only.

Query only command.

Returns the PathID for the current operating point of the instrument.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH?

SCPI Example

HARD:PATH?

Notes Return value is an integer.

State Saved

No

Initial S/W Revision

A.15.00

Retrieve Hardware PathID for Frequency and Mode

For M9484C

Remote command only.

Query only command.

Returns the PathID for the provided frequency and mode. For available modes, see Optimization Mode.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:FMODe? <frequency>,<integer_mode>

SCPI Example

HARD:PATH:FMOD? 1000000000,2 ! 1 GHz for mode 2

Notes

<frequency> is a floating point number with mHz resolution. Units such as GHz are not permitted.

Return value is an integer.

State Saved

No

Initial S/W Revision

A.15.00

Retrieve Hardware PathIDs for Mode

For M9484C

Remote command only.

Query only command.

Returns an integer list of PathIDs for the provided mode. For available modes, see Optimization Mode.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:MODE? <integer_mode>

SCPI Example

HARD:PATH:MODE? 2

State Saved

No

Initial S/W Revision

A.15.00

Set Hardware Path

For M9484C

Remote command only.

Sets the value for the PathID to be used for the provided Optimization Mode when the Enable Hardware Path is set to ON.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:SET <integer_mode>,<integer_path>

[:SOURce][:RF<channel>]:HARDware:PATH:SET?

SCPI Example

:HARD:PATH:SET 0,5

Preset

0,0

State Saved

Yes

Initial S/W Revision

A.15.00

Enable Hardware Path

For M9484C

Remote command only.

Enables or disables the setting of the PathID to the value entered with the Set Hardware Path command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:SET:ENABle ON|OFF|1|0

[:SOURce][:RF<channel>]:HARDware:PATH:SET:ENABle?

SCPI Example

:HARD:PATH:SET:ENAB?

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.15.00

Retrieve Hardware Band Transition Frequencies

For M9484C

Remote command only.

Query only command.

Returns a list of integers of frequencies (in Hz) where the instrument changes its internal RF hardware path or mixing products. The parameter supplied to the query refines the data retrieved by the query as listed below:

The number of entries in the list varies based on the parameter provided in the query.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:FREQuency:BTABle? ALL|P0|P1|P2|P3|P4|P5|P6|P7|P8|PMOD|PCUR|PALL

SCPI Example

:HARD:FREQ:BTAB? PMOD

State Saved

No

Initial S/W Revision

A.15.00

Offset Channel Level Flatness Data

For M9484C

Remote command only.

Sets an added response to the existing flatness data set; referred to as the ‘field copy’ of the alignment data. The parameters to the command are:

This command does not alter the factory calibration data. Performing Clear Channel Level Flatness Data Offsets will refresh the field copy of flatness from the factory calibration data. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:OFData <integer_path>,<data_block>

SCPI Example

:HARD:PATH:OFD 5,#2161000000,0.5,1.35 ! 1 MHz, 0.5 dB, 1.35 radians

State Saved

No

Initial S/W Revision

A.15.00

Clear Channel Level Flatness Data Offsets

For M9484C

Remote command only.

Clears any offsets previously applied to the existing flatness data set; referred to as the ‘field copy’ of the alignment data.

This command does not alter the factory calibration data. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:PATH:OFData:CLEar

SCPI Example

:HARD:PATH:OFD:CLE

State Saved

No

Initial S/W Revision

A.15.00

Set I/Q Delay Offset

For M9484C

Remote command only.

Applies the provided time delay to the I/Q Common Delay. This delay is in addition to the I/Q Common Delay in the Adjustments Block. The value of I/Q Common Delay in the Adjustment Block is not altered by setting this hardware I/Q offset.

This command is an absolute offset, meaning setting a new value overwrites any existing value.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:IQDelay <integer_path>,<value>

[:SOURce][:RF<channel>]:HARDware:CORRection:IQDelay? <integer_path>

SCPI Example

:HARD:CORR:IQD 5,0.000000003 ! Offset Path ID 5 with 3 ns

Notes

Value is seconds as a floating point number .

Min 0 s
Max 100 ns
Resolution 0.01 ps

Preset

N/A

State Saved

N/A

Initial S/W Revision

A.15.00

Clear I/Q Delay Offset

For M9484C

Remote command only.

Clears any previously provided time delay to the I/Q Common Delay. This clear will occur for all PathIDs. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:IQDelay:CLEar

SCPI Example

:HARD:CORR:IQD:CLE

State Saved

No

Initial S/W Revision

A.15.00

Set Phase Accumulator Delay Offset

For M9484C

Remote command only.

Applies the provided time delay to the Phase Accumulator . The Phase Accumulator determines the beginning time when all frequencies simultaneously have a zero phase – the origin for all frequencies phase ramps. Offsetting this time moves the coherent time origin.

This command is an absolute offset, meaning setting a new value overwrites any existing value.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:PADelay <integer_path>,<value>

[:SOURce][:RF<channel>]:HARDware:CORRection:PADelay? <integer_path>

SCPI Example

:HARD:CORR:PAD 5, 0.000000003 ! Offset Path ID 5 with 3 ns

Notes

Value is seconds as a floating point number.

Preset

N/A

State Saved

N/A

Min

0 s

Max

100 ns

Resolution

0.01 ps

Initial S/W Revision

A.15.00

Clear Phase Accumulator Delay Offset

For M9484C

Remote command only.

Clears any previously provided time delay to apply the Phase Accumulator. This clear will occur for all PathIDs. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:PADelay:CLEar

SCPI Example

:HARD:CORR:PAD:CLE

State Saved

No

Resolution

1 mradian

Initial S/W Revision

A.15.00

Set Phase Offset

For M9484C

Remote command only.

Applies the provided phase offset.

This command is an absolute offset, meaning setting a new value overwrites any existing value.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:POFFset <path_id>,<value>

[:SOURce][:RF<channel>]:HARDware:CORRection:POFFset? <path_id>

SCPI Example

:HARD:CORR:POFF 5,3 ! Offset Path ID 5 with 3 radians

Notes

Value is in radians as a floating point number.

Preset

N/A

State Saved

N/A

Min 0
Max 6.28

Resolution

1 mRadian

Initial S/W Revision

A.15.00

Clear Phase Offset

For M9484C

Remote command only.

Immediate action. Clears any previously provided phase offset. This clear will occur for all PathIDs. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:POFFset:CLEar

SCPI Example

:HARD:CORR:POFF:CLE

State Saved

No

Initial S/W Revision

A.15.00

Set Measured Baseband Delay

For M9484C

Remote command only.

Sets the delay to a channel’s baseband when two or more channels are in use and it is desired to have the basebands of each of these channels as closely aligned as possible. You can measure the offset of one channel from another, and then apply the correction to a channel with this command.

This command is an absolute offset, meaning setting a new value overwrites any existing value.

The delay within the instrument's circuitry can change when the firmware is updated. If you have characterized your system and established a value for Measured Baseband Delay with a particular firmware version, you may need to characterize the system and obtain a new value after updating firmware.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:MBDelay <value>

[:SOURce][:RF<channel>]:HARDware:CORRection:MBDelay?

SCPI Example

HARD:CORR:MBD 0.000000003

! Offsets channel 1 baseband by 3 ns

HARD:CORR:MBD?

Notes

Value is seconds as a floating point number .

Preset

This is unaffected by a Preset but is set to 0 on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Min

-1 us

Max

1 us

Resolution

0.01 ps

Initial S/W Revision

A.15.00

Modified at S/W Revision A.20.00 - Updated min and max values

Clear Measured Baseband Delay

For M9484C

Remote command only.

Clears previously provided measured baseband delay. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:CORRection:MBDelay:CLEar

SCPI Example

:HARD:CORR:MBD:CLE

State Saved

No

Initial S/W Revision

A.15.00

Update Quiescent Temperature

For M9484C

Remote command only.

Refreshes the quiescent temperature used for phase compensation at the time the Channel to Channel (C2C) correction is performed.

This command allows you to update the quiescent temperature for amplitude. However, this update is not a prerequisite for performing the C2C correction. It's important to note that the update of the quiescent temperature for amplitude is carried out during the Alignment process. Also, it is mandatory to run the Alignment before performing the Channel to Channel correction. There is no query form for the command.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:UQTemp AMPLitude|PHASe

SCPI Example

:HARD:UQT PHAS

State Saved

No

Initial S/W Revision

A.15.00

Retrieve Fundamental Frequency

For M9484C

Remote command only.

Query only.

Returns the fundamental frequency for the current state of the hardware.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:TFRequency:FUNDamental?

SCPI Example

HARD:TFR:FUND?

State Saved

No

Initial S/W Revision

A.17.00

Retrieve Frequency Translation Type

For M9484C

Remote command only.

Query only.

Returns the frequency translation type for the current state of the hardware as a string value.

SCPI Command

[:SOURce][:RF<channel>]:HARDware:TFRequency:TYPE?

SCPI Example

HARD:TFR:TYPE?

State Saved

No

Notes

Possible return values are:

  • High-side mixing

  • Low-side mixing

  • Direct

Initial S/W Revision

A.17.00