Fading

This capability requires at least one of the following license requirements to be met.

After selecting a channel configuration, waveform file (or real-time), and MIMO Order, the Fading graphical user-interface (GUI) presents you with a set of parameters for each signal path. The intended workflow progresses left to right, as available parameter selections are often dependent on what was selected prior (to left).

Enable Fading

MIMO Order

Copy Node (Signal 1/Output 1) to All Nodes

Function

Standard

Channel Model

Custom Profile

New Profile

Import Profile

Edit Profile

Select Profile

Update Profile

Delete Profile

Custom Profile List

Custom Profile List for Specified MIMO Order

Custom Profile List for Currently Selected MIMO Order

Correlation Matrix

Doppler Shift

Enable Fading

Enables or disables the fader processing for the specified Group. This control also appears on the Signal Summary screen.

GUI Location

Signals > Signal Summary selection > Fading Setup > Enable Fading

SCPI Command

[:SOURce]:GROup<group>:FADing ON|OFF|1|0

[:SOURce]:GROup<group>:FADing?

SCPI Example

GRO:FAD ON

GRO:FAD?

Notes

Setting cannot be set to On when the required Fading license(s) are not present or the specified Group’s Configuration is not supported. Supported Configuration Modes are Independent, MIMO2, and MIMO4.

Without the required Fading license(s), the following error is generated:

Attempting to set On will raise the error 703, "Feature not supported; Enable Fading unavailable. N7605AP0C or both F9860400A and N7605APPC are required."

Attempts to set a value not allowed will generate the following error:

-224,"Illegal parameter value"

Couplings

When Enable Fading is ON, maximum sample rate for the group is limited to 2.4 GHz.

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.10.00

Modified at S/W Version A.17.02 - License conditions changed

MIMO Order

Specifies the desired number of signals within the specified Group to apply fading to.  This is the N in NxM MIMO. This parameter also appears on the Signal Summary screen.

GUI Location

Signals > Signal Summary selection > Fading Setup > MIMO Order

SCPI Command

[:SOURce]:GROup<group>:FADing:MORDer 1|2|4|8

[:SOURce]:GROup<group>:FADing:MORDer?

SCPI Example

GRO:FAD:MORD 1

GRO:FAD:MORD?

Notes

Setting cannot be changed without Option 8SG.

Attempts to set a value not allowed will generate error:

-224,"Illegal parameter value"

The value of this setting will affect the available options for Channel Model, Correlation Matrix, and Doppler Shifts.

Preset

1

State Saved

Yes

Initial S/W Revision

A.10.00

Copy Node (Signal 1/Output 1) to All Nodes

GUI Option only

The Copy Node button copies the settings configured for the fading node - Signal 1/Output 1 to all other fading nodes which are configured by MIMO Order.

The following fading settings are copied to all fading nodes:

GUI Location

Signals > Signal Summary selection > Fading Setup > Copy Node (Signal 1/Output 1) to All Nodes

Initial S/W Revision

A.17.00

Function

Specifies the fader processing for the specified signal and RF Output.

GUI Location

Signals > Signal Summary selection > Fading Setup > Function

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:FUNCtion FADE|PASSthrough|OFF

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:FUNC?

SCPI Example

GRO:SIGN:FAD2:FUNC FADE

! This sets fading for the first signal in the first group’s output on the second RF Output.

GRO:SIGN:FAD2:FUNC?

Notes

Fading (FADing SCPI command parameter) cardinality is based upon the channels configured in the specified group.

Dependencies

Note the group Enable Fading setting supersedes this signal level fading function. If Enable Fading is not turned on for the group, the status of signal level fading function is ignored.

When Standard is set to Custom and the profile is not selected, attempting to set Function to Fade issues the error: -221, "Settings conflict; Function cannot be changed to Fade without a selected profile."

Couplings

Case 1 - Function is set to Fade, Standard is a value other than Custom, and the selected profile for custom fading is empty. In this case, if you set Standard to Custom, Function is automatically set to Passthrough.

Case 2 - Function is set to Fade, Standard is set to Custom, and the selected profile for custom fading becomes empty. In this case, Function is set to Passthrough.

Preset

PASS

Choices

FADE | PASSthrough | OFF

State Saved

Yes

Initial S/W Revision

A.10.00

Standard

Selects the radio standard for the specified fader. The standard models cover propagation environments that allow you to test whether your device meets the performance requirements as defined by the respective standard.

To set the Standard as Custom. the license models F9860400A and N7605APPC are required. When you set the Standard as Custom, you can import and select a custom fading profile for the fading setup.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:STANdard NR5G|LTE|CUSTom|NRNTN

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:STANdard?

SCPI Example

GRO:SIGN:FAD:STAN NR5G

GRO:SIGN:FAD:STAN?

Notes

Fading (FADing SCPI command parameter) cardinality is based upon the channels configured in each group.

For instruments without F9860400A and N7605APPC, attempting to set CUSTom issues the error:

  • +703,"Feature not supported;Custom Fading unavailable, F9860400A and N7605APPC are required."

For instruments without N7605AP0C, attempting to set NR5G or LTE issues the error:

  • +703,"Feature not supported; 3GPP MIMO fading (5GNR FR1 and FR2, LTE) unavailable, N7605AP0C is required."

For instruments without N7605AP0C with subscription date September 1, 2024, attempting to set NRNTN issues the error:

  • +703,"Feature not supported; NR NTN unavailable, N7605AP0C with subscription date September 1, 2024 is required. "

Dependencies

CUSTom requires F9860400A and N7605APPC.

NR5G and LTE require N7605AP0C.

NRNTN requires N7605AP0C with subscription date September 1, 2024.

Preset

NR5G

Range NR5G|LTE|Custom|NRNTN

State Saved

Yes

Initial S/W Revision

A.10.0

Modified S/W Revision

A.16.0 - Added CUSTom and NRNTN selections

A.17.0 - Added F9860400A as a required license to select CUSTom

A.17.02 - Added N7605AP0C as a required license to select NR5G and LTE

Channel Model

The channel model setting specifies the channel model (simulation type) for the specified fader. There are different models available for each standard. These are listed in detail below.

A channel model is a mathematical representation of the effects of a communication channel through which wireless signals are propagated. The channel model can represent the power loss incurred by the signal as it travels through the wireless medium to the receiver.

Channel Model options are:

GUI Location

Signals > Signal Summary selection > Fading Setup > Channel Model

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:CMODel STATic|TDLA10|TDLA30|TDLA100|TDLB100|TDLC5|TDLC300|TDLD10|TDLD30|EPA|ETU|EVA|SCEXSCS15K|SCEXSCS30K|SCE1SCS15K|SCE1SCS30K|SCE3SCS15K|SCE3SCS30K|SCE4SCS120k|SCEYSCS15K|SCEYSCS30K|SCEYSCS120K|SCEZSCS15K|SCEZSCS30K|SCE1|SCE3|MSCE1|MSCE2

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:CMODel?

SCPI Example

GRO:SIGN:FAD:CMOD TDLA30

GRO:SIGN:FAD:CMOD?

Notes

Attempts to set a value not allowed for the current instrument configuration and standard will generate error:

-224,"Illegal parameter value"

Fading (FADing SCPI command parameter) cardinality is based upon the channels configured in each group.

The models available for 5G are:

  • STATIC, TDLA10, TDLA30, TDLA100, TDLB100, TDLC5, TDLC300, TDLD10, TDLD30, SCEXSCS15K, SCEXSCS30K, SCE1SCS15K, SCE1SCS30K, SCE1SCS30K, SCE3SCS30K, SCE4SCS120K, SCEYSCS15K, SCEYSCS30K, SCEYSCS120K, SCEZSCS15K, SCEZSCS30K

The models available for LTE are:

  • STATIC, EPA, ETU, EVA, SCE1, SCE3, MSCE1, MSCE2

The models available for NR NTN are:

  • TDLA100, TDLC5, SCEXSCS15K, SCEXSCS30K

Dependencies

The set of allowed values depends upon the group configuration and standard.

Preset

STATIC

Choices

Static |TDLA10|TDLA30|TDLA100|TDLB100|TDLC300|TDLC5|TDLD10|TDLD30|EPA|ETU|EVA|SCEXSCS15K|SCEXSCS30K|SCE1SCS15K|SCE1SCS30K|SCESCS15K|SCE3SCS30K|SCE4SCS120K|SCEYSCS15K|SCEYSCS30K|SCEYSCS120K|SCEZSCS15K|SCEZSCS30K|SCE1|SCE3|MSCE1|MSCE2

State Saved

Yes

Initial S/W Revision

A.10.0

Custom Profile

The Custom Profile capability is available only for M9484C with N7605APPC.

When fading standard is set to Custom, this capability enables the use of custom fading profiles (*.tdlx files) that have been created and exported from the Channel Studio TDL application.

The Channel Studio TDL application is available in the PathWave Signal Generator software only when both N7605APPC with subscription date December 1, 2025, and F9860400A licenses are installed.

The instrument maintains a single, global list of custom fading profiles, regardless of which Group the file is imported from. From this list, a profile can be selected for the specified fading path.

New Profile

GUI option only.

Launches the Channel Studio TDL application to create a new custom fading profile. The Channel Studio TDL application gets launched and configured with the current MIMO filter parameters and frequency of RF channel.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard set to Custom > Select > Custom Fading Profile List screen > New Profile

SCPI Command

NA

Initial S/W Revision

A.19.00

Import Profile

Requires M9484C with both N7605APPC (subscription date December 1, 2025) and F9860400A

Imports a custom fading profile (.tdlx) file created using the Channel Studio TDL application.

Importing a profile adds the profile to the global list of custom fading profiles by copying the information from the .tdlx file. The .tdlx file name without the tdlx extension is used to name the imported profile. For example, if the 3GPP_5GNR_1x2_TDLA30_5_corrHigh.tdlx is used to import a profile, the imported profile name is 3GPP_5GNR_1x2_TDLA30_5_corrHigh.

If you are trying to import a fading profile (.tdlx) file which is not supported, an error similar to the one shown below is displayed. In such situations, you can click the Open Channel Studio button to access and customize/regenerate this file in the Channel Studio TDL application.

When using SCPI, attempting to import an unsupported fading profile issues the error: -200, "Execution error; Failed to import the profile. The specified TDLX file does not contain generated model for <model number>. Open the file with Channel Studio, set Platform matching your signal generator, press Generate Model, and import it into <model number> again."

There is no query form for this SCPI command.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard set to Custom > Select > Custom Fading Profile List screen > Import Profile

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:IMPort "filename"

SCPI Example

GRO:FAD:CUST:PROF:IMP "C:\abc\11 path Rician.tdlx"

State Saved

No

Initial S/W Revision

A.16.0

Edit Profile

GUI option only.

Launches the Channel Studio TDL application to edit the fading profile that you selected from the custom fading profiles list. The Channel Studio TDL application gets launched and configured with the fading profile that you currently selected in the imported profiles list.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard set to Custom > Select > Custom Fading Profile List screen > Edit Profile

SCPI Command

NA

Initial S/W Revision

A.19.00

Select Profile

Selects the custom fading profile when fading standard is set to Custom.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard set to Custom > Select > Custom Fading Profile List screen > Select

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<node>:CUSTom:PROFile <profile_name>

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:CUSTom:PROFile?

SCPI Example

GRO:SIGN:FAD:CUST:PROF "11 path Rician"

GRO:SIGN:FAD:CUST:PROF?

Notes

Available profiles are the imported profiles that match the currently selected MIMO order.

Attempting to set an unavailable profile raises the error: -220, "Parameter error; Cannot select an unavailable profile; must be imported and match the currently selected MIMO order. <profile_name>"

Couplings

When MIMO Order is changed, the custom profile name is reset to empty to allow you to select a custom profile as per the changed MIMO Order.

Preset

""

State Saved

Yes

Initial S/W Revision

A.16.00

Update Profile

Updates the currently selected profile with the specified .tdlx file. If the profile corresponding to the specified .tdlx file does not exist, a new profile is added.

There is no query form for the command.

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:UPDate "filename"

SCPI Example

GRO:FAD:CUST:PROF:UPD "C:\abc\11 path Rician.tdlx"

Couplings

When the currently selected profile is updated with the specified .tdlx file, this profile is continued to be used as the selected profile. Only the contents of the profile are updated with the specified .tdlx file.

State Saved

No

Initial S/W Revision

A.16.20

Delete Profile

Deletes the specified custom fading profile. There is no query form for this SCPI command.

GUI Location

Signals > Signal Summary selection > Fading Setup > Standard set to Custom > Select > Custom Fading Profile List screen > Delete

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:DELete <mimo order>,<profile_name>

SCPI Example

GRO:FAD:CUST:PROF:DEL "1x1","11 path Rician"

Notes

Attempting to set a value having an invalid format for <mimo order> issues the error: -220,"Parameter error; Invalid MIMO order format: <mimo_order>".

Attempting to delete the profile which does not exist issues the error: -220, "Parameter error; Specified profile does not exist. MIMO: <mimo order> , Name: <profile_name>".

Attempting to delete the profile which is currently selected issues the error: -200, "Execution error; Profile cannot be deleted while currently in use; MIMO: <mimo_order> , Name: <profile_name> "

Range

<mimo_order>: string of "MxN" format where M and N are positive integers

<profile_name>: string

State Saved

No

Initial S/W Revision

A.16.00

Custom Profile List

Remote Query only command.

Returns the list of imported custom fading profiles as a string of comma-separated values of MIMO orders and corresponding imported profile names. For example, if imported profiles are as follows:

The string returned for the above list of profiles is "1x1","Profile A","2x1","Profile B","4x2","Profile C".

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:LIST?

SCPI Example

GRO:FAD:CUST:PROF:LIST?

State Saved

No

Initial S/W Revision

A.16.00

Custom Profile List for Specified MIMO Order

Remote command only

Returns the list of imported custom fading profiles for the specified MIMO order. This command returns a string of comma-separated values for custom fading profile names.

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:LIST:MORDer? <mimo_order>

SCPI Example

GRO:FAD:CUST:PROF:LIST:MORD? "1x1"

Notes Attempting to set a value having an invalid format for <mimo_order> issues the error: -220,"Parameter error; Invalid MIMO order format: <mimo_order>".
Range <mimo_order>: string of "MxN" format where M and N are positive integers

State Saved

No

Initial S/W Revision

A.16.00

Custom Profile List for Currently Selected MIMO Order

Remote Query only command.

Returns the list of imported custom fading profiles for the currently selected MIMO order. This command returns a string of comma-separated values for custom fading profile names.

SCPI Command

[:SOURce]:GROup<group>:FADing:CUSTom:PROFile:LIST:MORDer:SELected?

SCPI Example

GRO:FAD:CUST:PROF:LIST:MORD:SEL?

State Saved

No

Initial S/W Revision

A.16.0

Correlation Matrix

The correlation matrix setting specifies the correlation level in spatial paths to use between the RF Outputs in the instrument group. In general, the higher the correlation between channels, the worse the "channel disparity". Because MIMO is banking on spatial differences in the channel to increase throughput, the higher correlated models represent worse conditions and subsequently lower throughput.
The correlation matrix settings are related to 3GPP standards. 5GNR base station conformance tests have correlations defined by 38.141-1 document in Annex G.

GUI Location

Signals > Signal Summary selection > Fading Setup > Correlation Matrix

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<node>:CMATrix NONE|LOW|MED|MEDA|HIGH|XPLOW|XPMED|XPMEDA|XPHIGH

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<node>:CMATrix

SCPI Example

GRO:SIGN:FAD:CMAT MEDA

GRO:SIGN:FAD:CMAT?

Notes

Attempts to set a value not allowed for the current instrument configuration and channel model will generate error:

-224,"Illegal parameter value"

Fading (FADing SCPI command parameter) cardinality is based upon the number of channels configured in the specified group.

XP is an abbreviation for cross polarization.

The "XPLOW|XPMED|XPMEDA|XPHIGH" settings are specifically calling out models that account for antenna cross-polarization in some capacity. It serves the same function as spatial correlation considerations, though it is calculated specifically for antenna effects.

Dependencies

The set of allowed values depends upon the group configuration and channel model.

For single RF output group configurations, NONE is the only available selection.

Preset

NONE

Choices

None|Low|Medium|Medium A|High|X Pol Low|X Pol Medium|X Pol Medium A|X Pol High

State Saved

Yes

Initial S/W Revision

A.10.00

Doppler Shift

This parameter specifies the doppler shift for the given fader. Doppler shift describes the changes in frequency of a propagated wave produced by a moving source with respect to an observer. Waves transmitted by an object traveling toward an observer get compressed resulting in a higher frequency as the source approaches the receiver.

GUI Location

Signals > Signal Summary selection > Fading Setup > Doppler Shift

SCPI Command

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:DSHift <freq>

[:SOURce]:GROup<group>:SIGNal<signal>:FADing<path>:DSHift?

SCPI Example

GRO:SIGN:FAD:DSH 75

!Sets the fader doppler shift to 75 Hz

GRO:SIGN:FAD:DSH?

Notes

Fading (FADing SCPI command parameter) cardinality is based upon the channels configured in each group.
There are limited sets of values for the current instrument configuration, standard, correlation matrix. The closest available value will be used from the fading profiles installed on the instrument.

Dependencies

The set of allowed values depends upon the group configuration, channel model, and correlation matrix.

Preset

0 Hz

State Saved

Yes

Min

0 Hz

Max

The min, max, and resolution are based upon the discrete values inside the fading profiles installed on the instrument. In other words, the actual value used will be quantized by the possibilities present.

The preset value above is the doppler shift value in the "STATIC" channel model, which is the preset channel model.

Initial S/W Revision

A.10.00

Signal Block

Signal Summary